Hello everybody:
I'm doing some range test with CC1200. I have two diffrent CC1200EM Kits: on 868/930MHz and 420/470Mhz with their respectiv antenas.
I'm using a proprietary evolution board wher i can switch the kits.
The problem/question:
My problem is that i do not know if i am using the right offset (99 for both right now)
At my desktop i have the rx and the tx in a distance of aprox. 1 m... beside of the tx i have a Aaronia spectral analyzer to verificate the values.
THE PROBLEM:
-If i use the 868 kit the values of RSSI give me around -70dBm. At the same time the spectral analyzer indicates me -32dBm
-If i use the 434 kit the values of RSSI gives me around -32dBm as well as the spectral analyzer.
Am i doing anything wrong with the offset at 868 KIt??? or is it right?????
I'm using 2-FSk @1,2bsps and 0dBm TX power. the rx fileter bw is at 14,88KHz.
Can anybody help me verifying the problem, if it is a problem .....
Thanks a lot