Part Number: CC1310
Other Parts Discussed in Thread: CC1190
Hello,
I have designed a board with an external RF Front End (Skyworks) with a typical gain of 16dB. I used it with SmartRF in two modes -- Configuring it as a regular CC1310 board and still enabling the GPIO for the Front End. With a transmitter kept within 1m range and transmitting at 14dBm (Launchpad) the RSSI in continuous RX is -15dBm.
However, if I change the module definition to a LaunchXL with Range Extender and then do the GPIO settings identical to above, the RSSI in continuous RX is -20dBm.
Is there an internal LNA which is turned-off when an external LNA is defined. What is the reason for the above behaviour.
Thanks,
Akshay