Other Parts Discussed in Thread: SMARTRFTM-STUDIO,
Hello,
We are testing the CC1125 using SMARTRFTM-STUDIO with the "Generic 434MHz Bit rate: 1.2kbps, 2-FSK, 12.5 kHz Channel spacing, optimized for sensitivity. (434MHz)" setting.
Looking at pages 13 and 15 in the datasheet (last row in the table), it says "image at -125 kHz." Can we take this to mean that the intermediate frequency (IF) should is 62.5 kHz? Is this a parameter that can be programmed in the device? What is the IFAMP register used for?
Regards,
Akash