Part Number: SIMPLELINK-CC3220-SDK
Dear SimpleLink Wi-Fi Developers -
The latest version SIMPLELINK-CC3220-SDK has been released here:
This version contains updates and additions which you will find useful and necessary - please download and use!
The most notable items are:
- Certificate catalog version 20171221.
- Added - Starfield Class 2 Certification Authority
- OTA - Critical bug fix
- Mandatory networking subsystem’s service pack fixing an issue in the signature verification of an OTA bundle that was intruduced in SDK version 1.50.0.6
- RTOS Demo apps:
- Local Time - Uses the new clock sync library to retrieve current local time, update the device time and set\get the local time zone for the device
- Libraries:
- SNTP - SNTP protocol implementation:
- Ability to retrive time information from a cloud NTP server
- Can provide a list of servers for automatic server choosing
- Clock Sync - CC32XX clock tools, supports the following:
- Update time using the SNTP library
- Update device time zone
- Update and retrive time from the networking subsystem’s clock using SNTP
- SLNETSock - a unified socket layer for the SimpleLink™ connected MCU product line for easy porting of networking libraries. This layer supports working with multiple physical interfaces and provides easy TLS and BSD API abstraction
- HTTP client - new library for HTTP client 1.0/1.1, supports the following features:
- Secured (HTTPS) connection
- HTTP GET,POST,HEAD,OPTIONS,PUT,DELETE,CONNECT methods
- Automatic redirect
- Automatic reconnect
- Setting persistant and non persistant request headers for a session
- Filtering response headers
- Chunked mode
- SNTP - SNTP protocol implementation:
- Host Driver:
- New API for Start TLS (see host driver API guide for further information)
- UniFlash Project Generator - a simple way to generate and program Uniflash projects (see README for further information)
- Please refer to the Documentation Overview for the individual release notes for details for each SDK component
- SimpleLink Platform level changes are available in SimpleLink Core SDK Release Notes
- SDK Change Log provides a list of all SDK component changes
Thanks and Best Regards for 2018!!!
JDW