Hi,
please find below a WLAN capture file of a ~10 Mbps TCP downlink traffic from AP to Android device using WL8. The WLAN connection between AP and the Android device is wired (WLAN antenna of Android device has been removed and RF cable has been connected to RF port, WLAN sniffer has been connected via directional coupler). Despite this ideal RF connection the Android device is once and then not able to receive WLAN packets. Please find below an example and the complete WLAN capture file. Do you have any explanation for these reception gaps?