Other Parts Discussed in Thread: WL1837
Tool/software: Linux
Hi All,
I am trying to evaluate the wl1837 module by configuring MESH + AP mode.
When I do start functionality after some time Wi-Fi is not functional as expected.
SETUP Details:
1. Driver and firmware version:
-> Using wlbuild version as "WL18xx_R8,7_SP1"
-> wlcore: PHY firmware version: Rev 8.2.0.0.237
-> wlcore: firmware booted (Rev 8.9.0.0.70)
Observations:
1. In mesh network there are 8 mesh nodes(8 AM437x-SK development based custom platforms and stopped communicating each other.
2. Stations are not able to connect APs which are initialized as virtual interface at all 8 AM437x-Sk development board based custom boards along with mesh functionality.
3. From the dmesg log identified the issue that dropping the received messages at driver level.
wlcore: WARNING corrupted packet in RX: status: 0x1 len: 118
[ 388.663234] wlcore: WARNING corrupted packet in RX: status: 0x1 len: 118
[ 389.198636] wlcore: WARNING corrupted packet in RX: status: 0x1 len: 70
[ 389.323340] wlcore: WARNING corrupted packet in RX: status: 0x1 len: 106
[ 389.468776] wlcore: WARNING corrupted packet in RX: status: 0x1 len: 70
[ 390.193721] wlcore: WARNING corrupted packet in RX: status: 0x1 len: 70
[ 474.199391] wlcore: WARNING corrupted packet in RX: status: 0x1 len: 118
[ 474.206364] wlcore: WARNING corrupted packet in RX: status: 0x1 len: 106
[ 474.791044] wlcore: WARNING corrupted packet in RX: status: 0x1 len: 70
[ 474.797983] wlcore: WARNING corrupted packet in RX: status: 0x1 len: 65
[ 474.804676] wlcore: WARNING corrupted packet in RX: status: 0x1 len: 65
[ 474.811593] wlcore: WARNING corrupted packet in RX: status: 0x1 len: 65
[ 474.895991] wlcore: WARNING corrupted packet in RX: status: 0x1 len: 118
4. From the driver I came to know reason for this drop packets could be of below reasons.
1. Received packet decryption failure (WL1271_RX_DESC_DECRYPT_FAIL)
2. memory-outage conditions
Looks in my case I am seeing the status as WL1271_RX_DESC_DECRYPT_FAIL.
5. I would like to know how can I resolve this issue.
Right now It was very critical issue for us to proceed further, Please suggest me how can i over right this issue.
Please provide me is there any patch which can help me to resolve this issue.
I appreciate your quick support on this issue.
Thanks & Regards
Ch. Siva