Team, Customer is using QNX OS on Sitara attempting certification using WL1833 and are experiencing issues.
Customer needs to configure WL1833 transmit bandwidth to be 20Mhz. Using Calibrator commands the outputs always show 20Mhz signals except when connected to an AP that supports 40Mhz then the WL1833 transmitted at 40Mhz bandwidth.
How do they specify bandwidth to 20MHz? Normally I would suggest the tune_channel command as discussed on the wiki, but I'm not sure if that's appropriate given they're using QNX processors.wiki.ti.com/.../WL18xx_TX_Testing