Hello,
I am looking for an alternative to the OPA140 which is capable of driving a higher capacitive load? My application is similar to the one in figure 3 of http://e2e.ti.com/blogs_/b/thesignal/archive/2012/03/21/differential-input-clamps-can-they-affect-your-op-amp-circuits.aspx
Due to the high slew rates in such an application, I would prefer to use an op amp without differential input clamp diodes.
The op amp is configured as unity buffer. The load resistance is 10kOhm and the load capacity is about 1.5nF.
The supply voltage is +14V and the negative supply is -12V. Furthermore, the application requires a slew rate >= 5V/µs.
The data sheet of the OPA140 recommends using a small resistor in series with the output for heavier capacitive loads. According to the accuracy requirement of my application, I cannot use a series resistor above 10Ohm.
Can you recommend me an alternative op amp fulfilling the above mentioned requirements? Or would you recommend using the four amplifiers of an OPA4140 in parallel?
Regards,
Steffen