Hello. This is my first time here. I have a little experience on DSP TMS320F28027 and I now plan to buy the DRV8301-HC-C2-KIT on which I have some questions.
1) Can it work as a "stand alone" device? I mean that after I do the adjustments needed for the motor, can I use it as a speed control without be connected with the PC?
2) Except for the POT integrated on the board are there any pins-out for outside board speed control?
3) On the insta-spin software can I set my 14-pole motor? Or I have to modify the source code for this?
4) What is the efficiency of this motor control kit (in which range it deviates)?
5) My motor delivers almost sinusoidal B-EMF on the oscilloscope. The insta-spin produces sinusoidal waveform or square for the motor 3-phases?
6) Is it possible to define the maximum frequency of the SPWM for the top speed?
7) Can I change the K (or A) coefficient (I mean the voltage to frequency 'linear' function) from the software or the source code?
8) Is it better to use the DRV8301-HC-C2-KIT or DRV8302-HC-C2-KIT; what is the main difference between them?
Thanks in advance.