Other Parts Discussed in Thread: DRA752
Tool/software: Linux
Hi all,
We have custom daughter board + custom DRA752 CPU module board with uboot 2014.07 in glsdk 7.03.00.00.3 , but some our CPU modules which filter out by our MP line are bad.
Because those CPU modules can not boot up successfully , the kernel panic has occurred during boot up, please reference the error log as below:
U-Boot 2014.07 (Apr 26 2017 - 16:16:36)
CPU : DRA752-GP ES2.0
Board: DRA7xx
I2C: ready
DRAM: 2 GiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1, OMAP SD/MMC: 2
Using default environment
serial# not set, setting...
SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Found 0 device(s).
SCSI: Net: Phy not found
cpsw
Hit any key to stop autoboot: 1 0
J6 ...
Card did not respond to voltage select!
Card did not respond to voltage select!
switch to partitions #0, OK
mmc1(part 0) is current device
SD/MMC found on device 1
reading j6_uenv.txt
206 bytes read in 2 ms (100.6 KiB/s)
Loaded environment from j6_uenv.txt
Importing environment from mmc1 ...
5178640 bytes read in 121 ms (40.8 MiB/s)
101700 bytes read in 8 ms (12.1 MiB/s)
Booting from mmc1 ...
Kernel image @ 0x82000000 [ 0x000000 - 0x4f0510 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8ffe4000, end 8ffffd43 ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 3.14.67-gb3b170c-dirty (andy@andy-Veriton-M490) (gcc version 4.7.3 20130226 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03) ) #2 SMP PREEMPT Wed Nov 30 21:05:59 CST 2016
[ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[ 0.000000] Machine model: TI DRA742 20161107
[ 0.000000] Reserved memory: created CMA memory pool at 0x95800000, size 56 MiB
[ 0.000000] Reserved memory: initialized node ipu2_cma@95800000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x99000000, size 64 MiB
[ 0.000000] Reserved memory: initialized node dsp1_cma@99000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x9d000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node ipu1_cma@9d000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x9f000000, size 8 MiB
[ 0.000000] Reserved memory: initialized node dsp2_cma@9f000000, compatible id shared-dma-pool
[ 0.000000] cma: CMA: reserved 64 MiB at ab800000
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] On node 0 totalpages: 518656
[ 0.000000] free_area_init_node: node 0, pgdat c0a575c0, node_mem_map ea7aa000
[ 0.000000] Normal zone: 1520 pages used for memmap
[ 0.000000] Normal zone: 0 pages reserved
[ 0.000000] Normal zone: 193536 pages, LIFO batch:31
[ 0.000000] HighMem zone: 2544 pages used for memmap
[ 0.000000] HighMem zone: 325120 pages, LIFO batch:31
[ 0.000000] DRA752 ES2.0
[ 0.000000] PERCPU: Embedded 8 pages/cpu @ea761000 s8640 r8192 d15936 u32768
[ 0.000000] pcpu-alloc: s8640 r8192 d15936 u32768 alloc=8*4096
[ 0.000000] pcpu-alloc: [0] 0 [0] 1
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 517136
[ 0.000000] Kernel command line: console=ttyO2,115200n8 elevator=noop root=/dev/mmcblk2p2 rw rootwait earlyprintk fixrtc omapdrm.num_crtc=2 consoleblank=0 cma=64M loglevel=8 rootfstype=ext4 snd.slots_reserved=1,1
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 1816504K/2074624K available (6799K kernel code, 692K rwdata, 2684K rodata, 376K init, 267K bss, 258120K reserved, 1300480K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xf0000000 - 0xff000000 ( 240 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xef800000 ( 760 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc094b0d4 (9485 kB)
[ 0.000000] .init : 0xc094c000 - 0xc09aa1c0 ( 377 kB)
[ 0.000000] .data : 0xc09ac000 - 0xc0a59260 ( 693 kB)
[ 0.000000] .bss : 0xc0a5926c - 0xc0a9bf7c ( 268 kB)
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] OMAP clockevent source: timer1 at 31475 Hz
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 65536000000000ns
[ 0.000030] OMAP clocksource: 32k_counter at 32768 Hz
[ 0.000427] Architected cp15 timer(s) running at 5.90MHz (virt).
[ 0.000463] sched_clock: 56 bits at 5MHz, resolution 169ns, wraps every 2911033065472ns
[ 0.000471] Switching to timer-based delay loop
[ 0.001517] Console: colour dummy device 80x30
[ 0.001534] WARNING: Your 'console=ttyO2' has been replaced by 'ttyS2'
[ 0.001542] This ensures that you still see kernel messages. Please
[ 0.001548] update your kernel commandline.
[ 0.001563] Calibrating delay loop (skipped), value calculated using timer frequency.. 11.80 BogoMIPS (lpj=59016)
[ 0.001577] pid_max: default: 32768 minimum: 301
[ 0.001688] Security Framework initialized
[ 0.001742] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001754] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.025728] CPU: Testing write buffer coherency: ok
[ 0.025982] /cpus/cpu@0 missing clock-frequency property
[ 0.026017] /cpus/cpu@1 missing clock-frequency property
[ 0.026029] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.026054] Setting up static identity map for 0x806a9808 - 0x806a9878
[ 0.080888] CPU1: Booted secondary processor
[ 0.080917] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[ 0.081052] Brought up 2 CPUs
[ 0.081068] SMP: Total of 2 processors activated (23.60 BogoMIPS).
[ 0.081076] CPU: All CPU(s) started in SVC mode.
[ 0.081502] devtmpfs: initialized
[ 0.082287] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[ 0.084005] omap_hwmod: l3_main_2 using broken dt data from ocp
[ 0.097310] omap_hwmod: tptc0 using broken dt data from edma-controller
[ 0.097827] omap_hwmod: tptc1 using broken dt data from edma-controller
[ 0.192234] omap_hwmod: dcan1: _wait_target_disable failed
[ 0.224996] omap_hwmod: tpcc: _wait_target_disable failed
[ 0.283250] pinctrl core: initialized pinctrl subsystem
[ 0.284010] regulator-dummy: no parameters
[ 0.288053] NET: Registered protocol family 16
[ 0.289874] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.292051] cpuidle: using governor ladder
[ 0.292062] cpuidle: using governor menu
[ 0.338984] syscon 4a002000.tisysconcore: regmap [mem 0x4a002000-0x4a0026cf] registered
[ 0.339326] syscon 4a002e00.tisyscon: regmap [mem 0x4a002e00-0x4a002e7b] registered
[ 0.342049] gpiochip_add: registered GPIOs 0 to 31 on device: gpio
[ 0.342313] OMAP GPIO hardware version 0.1
[ 0.343015] gpiochip_add: registered GPIOs 32 to 63 on device: gpio
[ 0.343846] gpiochip_add: registered GPIOs 64 to 95 on device: gpio
[ 0.344705] gpiochip_add: registered GPIOs 96 to 127 on device: gpio
[ 0.345591] gpiochip_add: registered GPIOs 128 to 159 on device: gpio
[ 0.346512] gpiochip_add: registered GPIOs 160 to 191 on device: gpio
[ 0.347404] gpiochip_add: registered GPIOs 192 to 223 on device: gpio
[ 0.348342] gpiochip_add: registered GPIOs 224 to 255 on device: gpio
[ 0.357018] platform 58820000.ipu: assigned reserved memory node ipu1_cma@9d000000
[ 0.357335] platform 55020000.ipu: assigned reserved memory node ipu2_cma@95800000
[ 0.357639] platform 40800000.dsp: assigned reserved memory node dsp1_cma@99000000
[ 0.376091] platform 41000000.dsp: assigned reserved memory node dsp2_cma@9f000000
[ 0.382459] No ATAGs?
[ 0.382485] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[ 0.382495] hw-breakpoint: maximum watchpoint size is 8 bytes.
[ 0.385448] OMAP DMA hardware revision 0.0
[ 0.415763] bio: create slab <bio-0> at 0
[ 0.431598] edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver
[ 0.437827] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver
[ 0.438479] of_get_named_gpiod_flags: can't parse gpios property of node '/fixedregulator-evm_3v3_sd[0]'
[ 0.438707] evm_3v3_sd: 3300 mV
[ 0.438820] of_get_named_gpiod_flags: can't parse gpios property of node '/fixedregulator-evm_3v3_sw[0]'
[ 0.439038] evm_3v3_sw: 3300 mV
[ 0.439101] reg-fixed-voltage fixedregulator-evm_3v3_sw: Failed to find supply vin
[ 0.439290] reg-fixed-voltage fixedregulator-evm_3v3_sw: Failed to register regulator: -517
[ 0.439310] platform fixedregulator-evm_3v3_sw: Driver reg-fixed-voltage requests probe deferral
[ 0.439363] of_get_named_gpiod_flags: can't parse gpios property of node '/fixedregulator-aic_dvdd[0]'
[ 0.439575] aic_dvdd: 1800 mV
[ 0.439631] reg-fixed-voltage fixedregulator-aic_dvdd: Failed to find supply vin
[ 0.439813] reg-fixed-voltage fixedregulator-aic_dvdd: Failed to register regulator: -517
[ 0.439832] platform fixedregulator-aic_dvdd: Driver reg-fixed-voltage requests probe deferral
[ 0.439885] of_get_named_gpiod_flags: can't parse gpios property of node '/fixedregulator-mmcwl[0]'
[ 0.440089] vmmcwl_fixed: 1800 mV
[ 0.440206] of_get_named_gpiod_flags: can't parse gpios property of node '/fixedregulator-vtt[0]'
[ 0.440411] vtt_fixed: 1350 mV
[ 0.440456] reg-fixed-voltage fixedregulator-vtt: Failed to find supply vin
[ 0.440645] reg-fixed-voltage fixedregulator-vtt: Failed to register regulator: -517
[ 0.440665] platform fixedregulator-vtt: Driver reg-fixed-voltage requests probe deferral
[ 0.444682] vgaarb: loaded
[ 0.445144] i2c-core: driver [palmas] using legacy suspend method
[ 0.445154] i2c-core: driver [palmas] using legacy resume method
[ 0.445757] SCSI subsystem initialized
[ 0.446190] libata version 3.00 loaded.
[ 0.447036] usbcore: registered new interface driver usbfs
[ 0.447204] usbcore: registered new interface driver hub
[ 0.447389] usbcore: registered new device driver usb
[ 0.449217] ======palmas_i2c_probe:526========
[ 0.449238] ======palmas_i2c_probe:559, features=0x0========
[ 0.449787] palmas 0-0058: IRQ missing: skipping irq request
[ 0.458256] palmas 0-0058: Muxing GPIO a, PWM 0, LED 0
[ 0.461414] prom_parse: Bad cell count for /ocp/i2c@48070000/tps659038@58
[ 0.484460] SMPS12: at 1070 mV
[ 0.501647] SMPS3: at 1350 mV
[ 0.537716] smps45: 850 <--> 1150 mV at 990 mV
[ 0.573766] smps6: 850 <--> 1250 mV at 1080 mV
[ 0.605608] smps7: 850 <--> 1060 mV at 1110 mV
[ 0.641669] smps8: 850 <--> 1250 mV at 1010 mV
[ 0.673506] smps9: 1800 mV
[ 0.695569] ldo1: 1800 <--> 3300 mV at 3000 mV
[ 0.721359] ldo2: 3300 mV
[ 0.751386] ldo3: 1800 mV
[ 0.767447] LDO4: no parameters
[ 0.776161] LDO5: no parameters
[ 0.784890] LDO6: no parameters
[ 0.793648] LDO7: no parameters
[ 0.802367] LDO8: no parameters
[ 0.821460] ldo9: 1050 mV
[ 0.851477] ldoln: 1800 mV
[ 0.881503] ldousb: 3300 mV
[ 0.893340] REGEN1: no parameters
[ 0.897820] regen2: no parameters
[ 0.909634] sysen1: no parameters
[ 0.918348] sysen2: no parameters
[ 0.922672] omap_i2c 48070000.i2c: bus 0 rev0.12 at 1 kHz
[ 0.923646] pcf857x 1-0026: probe error -121 for 'pcf8575'
[ 0.923665] pcf857x: probe of 1-0026 failed with error -121
[ 0.925158] omap_i2c 48072000.i2c: bus 1 rev0.12 at 400 kHz
[ 0.925597] omap_i2c 48060000.i2c: bus 2 rev0.12 at 1 kHz
[ 0.941570] pcf857x 3-0021: probe error -121 for 'pcf8575'
[ 0.941588] pcf857x: probe of 3-0021 failed with error -121
[ 0.941619] omap_i2c 4807a000.i2c: bus 3 rev0.12 at 1 kHz
[ 0.942070] omap_i2c 4807c000.i2c: bus 4 rev0.12 at 1 kHz
[ 0.942396] media: Linux media interface: v0.10
[ 0.942546] Linux video capture interface: v2.00
[ 0.942780] pps_core: LinuxPPS API ver. 1 registered
[ 0.942789] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.942905] PTP clock support registered
[ 0.944409] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
[ 0.944874] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
[ 0.946066] omap-iommu 40d01000.mmu: 40d01000.mmu registered
[ 0.946179] omap-iommu 40d02000.mmu: 40d02000.mmu registered
[ 0.946285] omap-iommu 58882000.mmu: 58882000.mmu registered
[ 0.946389] omap-iommu 55082000.mmu: 55082000.mmu registered
[ 0.946579] omap-iommu 41501000.mmu: 41501000.mmu registered
[ 0.946697] omap-iommu 41502000.mmu: 41502000.mmu registered
[ 0.947481] Advanced Linux Sound Architecture Driver Initialized.
[ 0.948913] Switched to clocksource arch_sys_counter
[ 0.968406] NET: Registered protocol family 2
[ 0.969129] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.969197] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.969329] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.969374] TCP: reno registered
[ 0.969387] UDP hash table entries: 512 (order: 2, 16384 bytes)
[ 0.969418] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[ 0.969617] NET: Registered protocol family 1
[ 0.969880] RPC: Registered named UNIX socket transport module.
[ 0.969889] RPC: Registered udp transport module.
[ 0.969897] RPC: Registered tcp transport module.
[ 0.969904] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.969914] PCI: CLS 0 bytes, default 64
[ 0.971141] hw perfevents: enabled with ARMv7 Cortex-A15 PMU driver, 7 counters available
[ 0.974221] futex hash table entries: 512 (order: 3, 32768 bytes)
[ 1.087359] bounce pool size: 64 pages
[ 1.087628] VFS: Disk quotas dquot_6.5.2
[ 1.087735] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 1.088352] NFS: Registering the id_resolver key type
[ 1.088386] Key type id_resolver registered
[ 1.088395] Key type id_legacy registered
[ 1.088429] jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
[ 1.088614] msgmni has been set to 1455
[ 1.092570] alg: No test for stdrng (krng)
[ 1.092750] NET: Registered protocol family 38
[ 1.092779] io scheduler noop registered (default)
[ 1.092789] io scheduler deadline registered
[ 1.092828] io scheduler cfq registered
[ 1.107298] pinctrl-single 4a003400.pinmux: 281 pins at pa fc003400 size 1124
[ 1.110472] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/axi@0/pcie@51000000[0]'
[ 1.123017] dra7-pcie 51000000.pcie: PCI host bridge to bus 0000:00
[ 1.123032] pci_bus 0000:00: root bus resource [io 0x1000-0x10000]
[ 1.123044] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
[ 1.123055] pci_bus 0000:00: No busn resource found for root bus, will use [bus 00-ff]
[ 1.123092] pci 0000:00:00.0: [104c:8888] type 01 class 0x060400
[ 1.123124] pci 0000:00:00.0: reg 0x10: [mem 0x00000000-0x000fffff]
[ 1.123148] pci 0000:00:00.0: reg 0x14: [mem 0x00000000-0x0000ffff]
[ 1.123212] pci 0000:00:00.0: supports D1
[ 1.123222] pci 0000:00:00.0: PME# supported from D0 D1 D3hot
[ 1.123573] PCI: bus0: Fast back to back transfers disabled
[ 1.123879] pci 0000:01:00.0: [8086:10d3] type 00 class 0x020000
[ 1.123926] pci 0000:01:00.0: reg 0x10: [mem 0x00000000-0x0001ffff]
[ 1.123957] pci 0000:01:00.0: reg 0x14: [mem 0x00000000-0x0000ffff]
[ 1.123986] pci 0000:01:00.0: reg 0x18: [io 0x0000-0x001f]
[ 1.124015] pci 0000:01:00.0: reg 0x1c: [mem 0x00000000-0x00003fff]
[ 1.124085] pci 0000:01:00.0: reg 0x30: [mem 0x00000000-0x0003ffff pref]
[ 1.124226] pci 0000:01:00.0: PME# supported from D0 D3hot D3cold
[ 1.124574] PCI: bus1: Fast back to back transfers disabled
[ 1.124589] pci_bus 0000:01: busn_res: [bus 01-ff] end is updated to 01
[ 1.124604] pci_bus 0000:00: busn_res: [bus 00-ff] end is updated to 01
[ 1.124731] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff]
[ 1.124747] pci 0000:00:00.0: BAR 8: assigned [mem 0x20200000-0x202fffff]
[ 1.124760] pci 0000:00:00.0: BAR 9: assigned [mem 0x20300000-0x203fffff pref]
[ 1.124772] pci 0000:00:00.0: BAR 1: assigned [mem 0x20020000-0x2002ffff]
[ 1.124786] pci 0000:00:00.0: BAR 7: assigned [io 0x1000-0x1fff]
[ 1.124802] pci 0000:01:00.0: BAR 6: assigned [mem 0x20300000-0x2033ffff pref]
[ 1.124814] pci 0000:01:00.0: BAR 0: assigned [mem 0x20200000-0x2021ffff]
[ 1.124834] pci 0000:01:00.0: BAR 1: assigned [mem 0x20220000-0x2022ffff]
[ 1.124853] pci 0000:01:00.0: BAR 3: assigned [mem 0x20230000-0x20233fff]
[ 1.124873] pci 0000:01:00.0: BAR 2: assigned [io 0x1000-0x101f]
[ 1.124892] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 1.124903] pci 0000:00:00.0: bridge window [io 0x1000-0x1fff]
[ 1.124915] pci 0000:00:00.0: bridge window [mem 0x20200000-0x202fffff]
[ 1.124926] pci 0000:00:00.0: bridge window [mem 0x20300000-0x203fffff pref]
[ 1.124943] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 1.124954] pci 0000:00:00.0: bridge window [io 0x1000-0x1fff]
[ 1.124965] pci 0000:00:00.0: bridge window [mem 0x20200000-0x202fffff]
[ 1.124976] pci 0000:00:00.0: bridge window [mem 0x20300000-0x203fffff pref]
[ 1.124990] pci_bus 0000:00: resource 4 [io 0x1000-0x10000]
[ 1.125000] pci_bus 0000:00: resource 5 [mem 0x20013000-0x2fffffff]
[ 1.125010] pci_bus 0000:01: resource 0 [io 0x1000-0x1fff]
[ 1.125020] pci_bus 0000:01: resource 1 [mem 0x20200000-0x202fffff]
[ 1.125029] pci_bus 0000:01: resource 2 [mem 0x20300000-0x203fffff pref]
[ 1.127378] OMAP DSS rev 6.1
[ 1.131707] panel-dpi display@2: GPIO lookup for consumer enable
[ 1.131718] panel-dpi display@2: using device tree for GPIO lookup
[ 1.131729] of_get_named_gpiod_flags: can't parse gpios property of node '/display@2[0]'
[ 1.131738] panel-dpi display@2: using lookup tables for GPIO lookup
[ 1.131748] panel-dpi display@2: lookup for GPIO enable failed
[ 1.132455] of_get_named_gpiod_flags exited with status 0
[ 1.132678] platform encoder@1: Driver dra7evm-tpd12s015 requests probe deferral
[ 1.133340] of_get_named_gpiod_flags: can't parse gpios property of node '/connector@1[0]'
[ 1.133383] connector-hdmi connector@1: failed to find video source
[ 1.133401] platform connector@1: Driver connector-hdmi requests probe deferral
[ 1.134341] pbias_mmc_omap5: 1800 <--> 3000 mV at 3000 mV
[ 1.135179] abb_mpu: 1100 <--> 1210 mV
[ 1.135536] abb_ivahd: 1060 <--> 1250 mV
[ 1.135903] abb_dspeve: 1060 <--> 1250 mV
[ 1.136268] abb_gpu: 1060 <--> 1280 mV
[ 1.137451] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 1.141703] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/serial@4806a000[0]'
[ 1.142111] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 299, base_baud = 3000000) is a 8250
[ 1.142509] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/serial@4806c000[0]'
[ 1.142873] 4806c000.serial: ttyS1 at MMIO 0x4806c000 (irq = 300, base_baud = 3000000) is a 8250
[ 1.143302] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/serial@48020000[0]'
[ 1.143663] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 301, base_baud = 3000000) is a 8250
[ 2.793318] console [ttyS2] enabled
[ 2.797273] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/serial@48066000[0]'
[ 2.806658] 48066000.serial: ttyS4 at MMIO 0x48066000 (irq = 302, base_baud = 3000000) is a 8250
[ 2.815923] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/serial@48068000[0]'
[ 2.825295] 48068000.serial: ttyS5 at MMIO 0x48068000 (irq = 303, base_baud = 3000000) is a 8250
[ 2.834572] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/serial@48424000[0]'
[ 2.843951] 48424000.serial: ttyS8 at MMIO 0x48424000 (irq = 304, base_baud = 3000000) is a 8250
[ 2.853211] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/serial@4ae2b000[0]'
[ 2.862587] 4ae2b000.serial: ttyS9 at MMIO 0x4ae2b000 (irq = 305, base_baud = 3000000) is a 8250
[ 2.873349] omap_rng 48090000.rng: OMAP Random Number Generator ver. 20
[ 2.880560] [drm] Initialized drm 1.1.0 20060810
[ 2.895865] brd: module loaded
[ 2.904475] loop: module loaded
[ 2.907986] (hci_tty): inside hci_tty_init
[ 2.912469] (hci_tty): allocated 249, 0
[ 2.918961] ahci 4a140000.sata: SSS flag set, parallel bus scan disabled
[ 2.925712] ahci 4a140000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
[ 2.934295] ahci 4a140000.sata: flags: 64bit ncq sntf stag pm led clo only pmp pio slum part ccc apst
[ 2.944801] scsi0 : ahci_platform
[ 2.948620] ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a1410ff] port 0x100 irq 343
[ 2.957950] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 2.973986] usbcore: registered new interface driver asix
[ 2.979575] usbcore: registered new interface driver ax88179_178a
[ 2.985830] usbcore: registered new interface driver cdc_ether
[ 2.991867] usbcore: registered new interface driver smsc95xx
[ 2.997773] usbcore: registered new interface driver net1080
[ 3.003618] usbcore: registered new interface driver cdc_subset
[ 3.009732] usbcore: registered new interface driver zaurus
[ 3.015495] usbcore: registered new interface driver cdc_ncm
[ 3.022120] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 3.028678] ehci-pci: EHCI PCI platform driver
[ 3.033298] ehci-omap: OMAP-EHCI Host Controller driver
[ 3.039118] usbcore: registered new interface driver cdc_wdm
[ 3.044958] usbcore: registered new interface driver usb-storage
[ 3.051337] usbcore: registered new interface driver usbserial
[ 3.057336] usbcore: registered new interface driver pl2303
[ 3.063083] usbserial: USB Serial support registered for pl2303
[ 3.070197] mousedev: PS/2 mouse device common for all mice
[ 3.078243] i2c-core: driver [rtc-ds1307] using legacy suspend method
[ 3.084730] i2c-core: driver [rtc-ds1307] using legacy resume method
[ 3.091808] rtc rtc0: 48838000.rtcss: dev (254:0)
[ 3.096547] omap_rtc 48838000.rtcss: rtc core: registered 48838000.rtcss as rtc0
[ 3.104916] i2c /dev entries driver
[ 3.110090] ov1063x 1-0037: ov1063x Product ID 0 Manufacturer ID 0
[ 3.117241] vpe 489d0000.vpe: loading firmware vpdma-1b8.bin
[ 3.123438] vip 48990000.vip: No explicit pinctrl resources data.
[ 3.130519] vip 48990000.vip: loading firmware vpdma-1b8.bin
[ 3.137015] of_get_named_gpiod_flags exited with status 0
[ 3.142551] DRA7xx Radio probe done
[ 3.146240] vpe 489d0000.vpe: Device registered as /dev/video0
[ 3.152128] vip 48990000.vip: VPDMA firmware loaded
[ 3.157046] vip2-s0: Port A enabled but no endpoints found
[ 3.162460] vip2-s1: Port A enabled but no endpoints foundvip2-s0: Port B enabled but no endpoints found
[ 3.172139] Driver for 1-wire Dallas network protocol.
[ 3.172150] vip2-s1: Using subdev ov1063x 1-0037 for capture
[ 3.172439] vip2-s1: vip Device registered as /dev/video1
[ 3.189876] coproc iva_coproc: probe
[ 3.193568] Adding alias for supply vdd,iva_coproc -> vdd,4a0025cc.voltdm
[ 3.200412] Adding alias for supply vbb,iva_coproc -> vbb,4a0025cc.voltdm
[ 3.227929] coproc iva_coproc: coproc_probe result=0
[ 3.232973] coproc dsp_coproc: probe
[ 3.236650] Adding alias for supply vdd,dsp_coproc -> vdd,4a0025e0.voltdm
[ 3.243512] Adding alias for supply vbb,dsp_coproc -> vbb,4a0025e0.voltdm
[ 3.270954] coproc dsp_coproc: coproc_probe result=0
[ 3.280306] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 3.289015] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/mmc@4809c000[0]'
[ 3.297754] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/mmc@4809c000[0]'
[ 3.298970] ata1: SATA link down (SStatus 0 SControl 300)
[ 3.359127] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/mmc@480b4000[0]'
[ 3.367904] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/mmc@480b4000[0]'
[ 3.376965] omap_hsmmc 480b4000.mmc: unable to get vmmc regulator -517
[ 3.383612] platform 480b4000.mmc: Driver omap_hsmmc requests probe deferral
[ 3.390824] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/mmc@480d1000[0]'
[ 3.399615] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/mmc@480d1000[0]'
[ 3.408611] 480d1000.mmc supply vmmc not found, using dummy regulator
[ 3.415411] omap_hsmmc 480d1000.mmc: could not set regulator OCR (-22)
[ 3.459694] ledtrig-cpu: registered to indicate activity on CPUs
[ 3.466048] omap-aes 4b500000.aes: OMAP AES hw accel rev: 3.3
[ 3.472361] alg: skcipher: Test 4 failed on encryption for ecb-aes-omap
[ 3.479056] 00000000: e7 aa a4 c2 69 29 cc 22 2c fd 0d c7 02 6e 6f 39
[ 3.485561] 00000010: 56 1e c2 b2 f6 a1 66 58 b8 65 c3 d8 5e 0f b4 a4
[ 3.492078] 00000020: 5e 06 f0 5f 31 51 18 37 45 d7 ca 3a fd 6c 3f e1
[ 3.498555] 00000030: dd 8d 22 65 2b 00 50 ce ba 28 67 d7 ce 0e 0d ea
[ 3.505043] 00000040: 6c 22 0b fe ed 75 1d df 64 7d c5 33 68 32 cf 00
[ 3.505053] omap_hsmmc 480d1000.mmc: exceeding card's volts
[ 3.517119] 00000050: cb 6d a2 fb da af 09 f8 81 82 27 fa 45 9c 29 a4
[ 3.523667] 00000060: 50 59 93 15 4b 9d 4e 9d 2c 7f 9e cf 64 98 72 c4
[ 3.530158] 00000070: 41 72 51 97 1d 07 49 a0 1b 8e 65 4b b2 6a 12 03
[ 3.536634] 00000080: a0 d4 a7 c0 c0 5f ef 47 ad 2a 98 03 b3 4f 33 66
[ 3.543113] 00000090: 22 74 a6 6c 9b 73 ce 3f e1 8b 22 17 59 0c 47 89
[ 3.549600] 000000a0: 33 a1 d6 47 03 19 4f a8 67 69 f0 5b f0 20 ad 06
[ 3.556074] 000000b0: 32 7f b5 ba 56 16 00 bc 10 88 37 44 07 9e 55 e7
[ 3.562561] 000000c0: 12 2f 07 32 ee 39 af 64 05 8f b3 d4 eb 1b 46 6e
[ 3.569038] 000000d0: 41 70 2e cd 52 2d 46 8c 18 d1 2e 16 97 35 57 f0
[ 3.575513] 000000e0: bd 0a 14 95 0f 8b a8 2f 4b 1b a7 bf 82 a6 43 0c
[ 3.582002] 000000f0: b9 39 4a a8 10 6f 50 7b 25 fb 26 81 e0 2f f0 96
[ 3.588470] 00000100: 21 3e 8c 1b 16 55 8d a1 17 5a 02 de b1 55 f6 6d
[ 3.594949] 00000110: fc a0 d9 bf 7c 3a 0e 29 6f d1 6c 6f a5 da bf b1
[ 3.601434] 00000120: 84 a5 e2 5a 03 12 29 c8 1c b3 99 c4 c4 10 aa 97
[ 3.607909] 00000130: f0 f6 f0 59 bd 8f 38 50 31 cb 69 3f 96 15 d6 f5
[ 3.614399] 00000140: 4b 17 24 f5 9f 1f af e2 be 52 83 10 60 53 e4 6f
[ 3.620887] 00000150: dc 6a 80 34 73 97 1b c5 ca 26 16 77 0e 60 ab 89
[ 3.627362] 00000160: 0f 04 27 bd ce 3e 71 b4 a0 d7 22 7e db eb 24 70
[ 3.633849] 00000170: 6d 2d d9 3c fa e7 ea d5 5a 4c a4 b0 a7 17 e8 41
[ 3.640338] 00000180: 11 08 42 4f e5 ad 26 92 d2 00 ae a8 e3 4b 37 47
[ 3.646823] 00000190: f6 36 a3 36 c5 7e 00 78 0a 39 b7 ea d0 6a 16 1c
[ 3.653312] 000001a0: 35 a2 fd 45 52 39 13 6f c1 53 f3 53 df 33 84 d7
[ 3.659808] 000001b0: d2 c8 37 b0 75 e3 41 46 b3 c7 83 2e 8a bb a4 e5
[ 3.666291] 000001c0: 6a b0 a9 fc a0 0f 61 66 e1 6d 2b 75 06 0a fd 27
[ 3.666304] mmc1: host does not support reading read-only switch. assuming write-enable.
[ 3.680905] 000001d0: 40 86 7f 51 e1 11 9c cb 88 e6 68 47 e3 2b c5 ff
[ 3.680926] omap_hsmmc 480d1000.mmc: no pinctrl state for hs or hs-rev20 mode
[ 3.680937] omap_hsmmc 480d1000.mmc: no pinctrl state for hs or hs-rev20 mode
[ 3.701711] 000001e0: 02 27 02 3f ef ac ce 31 d0 86 81 9b 6d 22 c1 cf
[ 3.708204] omap_hsmmc 480d1000.mmc: no pinctrl state for hs or hs-rev20 mode
[ 3.709230] alg: skcipher: Test 1 failed on encryption for ctr-aes-omap
[ 3.709234] 00000000: 87 4d 61 91 b6 20 e3 26 1b ef 68 64 98 0d b6 ce
[ 3.709238] 00000010: 98 06 f6 6b 79 70 fd ff 86 17 18 7b b9 ff fd ff
[ 3.709241] 00000020: 5a e4 df 3e db d5 d3 5e 5b 4f 09 02 0c b0 3e ab
[ 3.709245] 00000030: 1e 03 1d da 2f be 03 d1 79 21 70 a0 f3 00 9c ee
[ 3.709292] Unable to handle kernel NULL pointer dereference at virtual address 0000001e
[ 3.709296] pgd = c0004000
[ 3.709302] [0000001e] *pgd=00000000
[ 3.709308] Internal error: Oops: 5 [#1] PREEMPT SMP ARM
[ 3.709313] Modules linked in:
[ 3.709320] CPU: 0 PID: 1078 Comm: cryptomgr_test Not tainted 3.14.67-gb3b170c-dirty #2
[ 3.709325] task: e99fc040 ti: e9d30000 task.ti: e9d30000
[ 3.709336] PC is at omap_aes_gcm_crypt+0x6c/0x230
[ 3.709348] LR is at crypto_mod_put+0x54/0x58
[ 3.709354] pc : [<c0544ad4>] lr : [<c02744c4>] psr: 20000113
[ 3.709354] sp : e9d31cd0 ip : e9d31c08 fp : e9d31d3c
[ 3.709358] r10: e9b10168 r9 : e9d2d000 r8 : e9b10100
[ 3.709362] r7 : 00000001 r6 : fffffffe r5 : e9b10080 r4 : e9d31ce8
[ 3.709366] r3 : 00000006 r2 : 0000000c r1 : 000000d0 r0 : fffffffe
[ 3.709371] Flags: nzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment kernel
[ 3.709375] Control: 10c5387d Table: 8000406a DAC: 00000015
[ 3.709380] Process cryptomgr_test (pid: 1078, stack limit = 0xe9d30240)
[ 3.709384] Stack: (0xe9d31cd0 to 0xe9d32000)
[ 3.709389] 1cc0: c09f2f38 00000000 c0a59ed8 00000010
[ 3.709396] 1ce0: 00000011 e9b10100 01000000 e9d31cf8 c0028cfc e9b10100 00000010 e9b10100
[ 3.709402] 1d00: c0a83b00 e9b10148 00000010 c0545030 0000000f 00000000 00000000 e9daa000
[ 3.709407] 1d20: 00000001 e9b10100 e9d2d000 c0a137a8 e9d31d4c e9d31d40 c0544fe0 c0544a74
[ 3.709413] 1d40: e9d31e7c e9d31d50 c027e6a0 c0544fd8 e9aefcc0 00000000 e9aefd00 c002b618
[ 3.709419] 1d60: e9d31d84 e9d31d70 00000010 c002a158 e9aeb210 c0a42770 e9d31d9c c08946a8
[ 3.709425] 1d80: c089980c e9d89440 60000193 00000000 e9d893c0 e9d31da0 c06a47e0 e9d89340
[ 3.709431] 1da0: e9b10100 00000001 00000009 e9b10080 00000000 c0a137a8 e9d31ddc 00000000
[ 3.709436] 1dc0: 00000000 e9d31dc4 e9d31dc4 e9aeb270 e9daa000 e9da9000 e9da8000 e9d27000
[ 3.709442] 1de0: e9d26000 e9d25000 e9d24000 e9d23000 e9d31e84 e9d31e00 c0276e94 e9aeb210
[ 3.709447] 1e00: e9aeb270 00000004 e9d31e24 e9d31e18 e9d2d000 e9d72000 e9d73000 e9d62000
[ 3.709453] 1e20: e9d63000 e9c14000 e9c15000 e9d02000 00000000 00000000 00000000 01000000
[ 3.709458] 1e40: 00000000 00000000 00000000 00000000 00000000 e9b10100 00000009 c0a137a8
[ 3.709464] 1e60: 00000001 e9d5f6c0 00000000 e9d5f700 e9d31eac e9d31e80 c027f14c c027e344
[ 3.709470] 1e80: 00000000 00000000 c06c90cc c06c90cc e9b10100 00000000 e9d5f6c0 e9d5f6c0
[ 3.709476] 1ea0: e9d31ecc e9d31eb0 c027f24c c027f128 ffffffff 0000005c 00000000 00001083
[ 3.709482] 1ec0: e9d31f44 e9d31ed0 c027f70c c027f1e4 c09a9ac0 00000400 c006dfe8 c006dd28
[ 3.709488] 1ee0: e9d31f24 e9d31ef0 c007aa80 e9d30000 e9923c40 a0000113 c027c418 00000000
[ 3.709493] 1f00: 00000000 00000000 e9d31f2c e9d31f18 c06a199c c06a135c 00000002 e9d5f6c0
[ 3.709500] 1f20: e9dbd140 e9d5f6c0 c027c418 00000000 00000000 00000000 e9d31f5c e9d31f48
[ 3.709505] 1f40: c027c444 c027f534 e99fc040 00000000 e9d31fac e9d31f60 c0062798 c027c424
[ 3.709511] 1f60: e9d31f94 00000000 c006a498 e9d5f6c0 00000000 00000000 e9d31f78 e9d31f78
[ 3.709516] 1f80: 00000000 00000000 e9d31f88 e9d31f88 e9dbd140 c00626c0 00000000 00000000
[ 3.709522] 1fa0: 00000000 e9d31fb0 c000ec00 c00626cc 00000000 00000000 00000000 00000000
[ 3.709527] 1fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 3.709533] 1fe0: 00000000 00000000 00000000 00000000 00000013 00000000 00dcd38a 423e6fb4
[ 3.709537] Backtrace:
[ 3.709546] [<c0544a68>] (omap_aes_gcm_crypt) from [<c0544fe0>] (omap_aes_gcm_encrypt+0x14/0x18)
[ 3.709561] r10:c0a137a8 r9:e9d2d000 r8:e9b10100 r7:00000001 r6:e9daa000 r5:00000000
[ 3.709565] r4:00000000
[ 3.709577] [<c0544fcc>] (omap_aes_gcm_encrypt) from [<c027e6a0>] (__test_aead+0x368/0xde4)
[ 3.709587] [<c027e338>] (__test_aead) from [<c027f14c>] (test_aead+0x30/0xbc)
[ 3.709599] r10:e9d5f700 r9:00000000 r8:e9d5f6c0 r7:00000001 r6:c0a137a8 r5:00000009
[ 3.709604] r4:e9b10100
[ 3.709613] [<c027f11c>] (test_aead) from [<c027f24c>] (alg_test_aead+0x74/0xac)
[ 3.709625] r8:e9d5f6c0 r7:e9d5f6c0 r6:00000000 r5:e9b10100 r4:c06c90cc
[ 3.709633] [<c027f1d8>] (alg_test_aead) from [<c027f70c>] (alg_test+0x1e4/0x284)
[ 3.709643] r7:00001083 r6:00000000 r5:0000005c r4:ffffffff
[ 3.709650] [<c027f528>] (alg_test) from [<c027c444>] (cryptomgr_test+0x2c/0x4c)
[ 3.709662] r10:00000000 r9:00000000 r8:00000000 r7:c027c418 r6:e9d5f6c0 r5:e9dbd140
[ 3.709666] r4:e9d5f6c0
[ 3.709678] [<c027c418>] (cryptomgr_test) from [<c0062798>] (kthread+0xd8/0xe4)
[ 3.709684] r4:00000000 r3:e99fc040
[ 3.709694] [<c00626c0>] (kthread) from [<c000ec00>] (ret_from_fork+0x14/0x34)
[ 3.709704] r7:00000000 r6:00000000 r5:c00626c0 r4:e9dbd140
[ 3.709711] Code: e50b3058 ebf4cc44 e3a010d0 e1a06000 (e5900020)
[ 3.709728] ---[ end trace 35c2627f99968ff2 ]---
[ 4.188073] mmc1: new high speed SDHC card at address 1234
[ 4.194110] mmcblk1: mmc1:1234 SA04G 3.70 GiB
[ 4.199890] mmcblk1: p1 p2
[ 17.776451] ata1: exception Emask 0x10 SAct 0x0 SErr 0x4050002 action 0xe frozen
[ 17.783898] ata1: irq_stat 0x00000040, connection status changed
[ 17.789947] ata1: SError: { RecovComm PHYRdyChg CommWake DevExch }
[ 17.796169] ata1: hard resetting link
[ 27.788938] ata1: softreset failed (1st FIS failed)
[ 27.793840] ata1: hard resetting link
[ 33.578955] ata1: SATA link down (SStatus 0 SControl 300)
[ 33.584390] ata1: EH complete
Could you give us some direction to debug it ? ( it should be h/w issue , but we want to know which part is NG )
BTW, I have increased debug level (loglevel=8) in j6_uenv.txt.
Best Regards,
Bowei Ren