Hi,
I just wonder if Timer 6 (ball A11) and Timer 7 (ball B13) of DRA750/DRA755 can be programmed as PWM input or output?
If yest, what is the limit for the frequency and duty cycle of this PWM?
And if I use two DRA750 (or DRA755) and have the same timer connected ,I mean SOC1 BALL A11(B13) connected to SOC2 BALL A11(B13),then program the PWM on SOC1 as output and that on SOC2 as input,
can SOC2 detect PWM signal from SOC1?
For our system,SOC1 is the DUT and SOC2 is the CPU on test fixture to verify the functions of SOC1.