Other Parts Discussed in Thread: DRA742, PMP, DRA752, TVP5158
Tool/software: Linux
Hi,
I have an older J6 EVM board that works very well with the previous PSDKLA (v03.02.00.03) but when I use the new PSDKLA (v03.04.00.03) there are 3 failures reported during the boot process. I've rechecked my build process and I don't think I've missed anything. I'm wondering if my board is not compatible with the new PSDKLA.
My board identification number is:
CPU : DRA752-GP ES1.1
Model: TI DRA742
Board: DRA74x EVM REV G.0
DRAM: 1.5 GiB
The 3 errors that occur during the boot process is:
[FAILED] Failed to start Load Kernel Modules.
[FAILED] Failed to start Synchronize System and HW clocks.
[FAILED] Failed to start TI MultiCore Tools Daemon.
Thanks,
Todd