Part Number: TDA3
Tool/software: Code Composer Studio
I was trying to flash the M4 with a program using JTAG , in the user guide as well as on similar board I am getting MID - 1 DID – 18, but on a particular board I am getting it as MID - FF DID -FF.
The JTAG is also failing at location 0x00, and stops immediately without flashing...showing below logs
Read xxxxxx bytes from [100%] file...Done.
QSPI whole chip erase in progress
QSPI file write started
QSPI file write failed at 0x00
************QSPI flash completed sucessfully**************
Can please tell me what is the issue..
Thank You