Hello,
For a lane detection algorithm I want to use the VLIB_houghLineFromList() from VLIB. I'm working on a TDA3x and the algo should run on a C66x DSP.
My question is: How do I get the houghLineFromList function to produce correct theta and rho values? Let's say in my case i have an image/ROI of 1920x500 pixel. How do I choose the right values for NUMTHETA and RHOMAX to get correct results? If I want theta to range from -90° to 89° do I simply set NUMTHETA to 180? And should I set RHOMAX to 2*sqrt(W^2 + H^2)?
I looked at the HoughLinesDemo included in the VLIB release and couldn't really understand why you choose the values 267(NUMTHETA) and 600 (RHOMAX). I also searched through the e2e forums, but unfortunately I couldn't find an answer. I'm using vlib_c66x_3_3_0_3.
Thanks in advance,
Tobias