Hello,
I'm using the new version of TIDL00.08 ,and try to import the model.
And from the source code I know we have to build a config file and then put the file name and parameter in it.
But I try but it can not catch my net name in the config file.as below.
inside my config_file.txt:
I
my cmd show
It seems that It catch the config file but can not catch the net file name inside.
It even can not print the string of my net.
I change a lot of format in the config file and try,but it still didn't work.
And is there have any training video or doc about the new version of TIDL?
It may be useful for me if any.
Thanks in advance.
Best regards,
Jimmy Lai