Hi:
I use VisionSDK_03_02_00_00,and try to run the tidl demo "Semantic_Segmentation";the system is booted OK,and I can see the vision SDK Usecases menu:
[IPU1-0] 1: Single Camera Usecases
[IPU1-0] 2: Multi-Camera LVDS Usecases
[IPU1-0] 3: AVB RX Usecases, (TDA2x & TDA2Ex ONLY)
[IPU1-0] 4: Dual Display Usecases, (TDA2x EVM ONLY)
[IPU1-0] 5: ISS Usecases, (TDA3x ONLY)
[IPU1-0] 6: TDA2x Stereo Usecases
[IPU1-0] 7: Network RX/TX Usecases
[IPU1-0] a: Miscellaneous test's
[IPU1-0] c: OPENVX Usecases
[IPU1-0] f: TIDL File I/O Usecase
[IPU1-0] g: Semantic Segmentation Usecase
But when I enter "g",the error is reported:
[IPU1-0] 60.286524 s: Assertion @ Line: 1500 in nullSrcLink_tsk.c: pObj->fpDataStream[chId] != SYSTEM_LINK_STATUS_EFAIL : failed !!!
[IPU1-0] 60.287165 s: Assertion @ Line: 1500 in nullSrcLink_tsk.c: pObj->fpDataStream[chId] != SYSTEM_LINK_STATUS_EFAIL : failed !!!
Of course,I put the "TIDLCFG.TXT "、"IN.RGB "、"PRM.BIN "、"NET.BIN " four files in the root of SD.
Is the “In.RGB” is same as used in "TIDL File I/O Usecase",or other format file?
What am I missing? Or something else wrong?
Pls help me!