Hi
Reading the AM335x TRM, I see that there are two IRQ associated to GPIO0/1/2/3.
For a example of GPIO3: there are the related Registers:
GPIO_IRQSTATUS_RAW_0
GPIO_IRQSTATUS_RAW_1
GPIO_IRQSTATUS_0
GPIO_IRQSTATUS_1
GPIO_IRQSTATUS_SET_0
GPIO_IRQSTATUS_SET_1
・・・・
My question is that:
What is the difference between the "XXX_0" and "XXX_1"?
Why are there two synchronous interrupt requests 1 and 2 ?
How can I proper use them?
For example, when the GPIO3_7 Low Level is detected,
GPIO_IRQSTATUS_RAW_0 and GPIO_IRQSTATUS_RAW_1, which of the registers will be set?
Thanks!