Hi,
The ethercat_slave project default is syncmanager + dc mode.
Have you ever configure the ethercat_slave project to FREERUN + DC mode on AM335x_ICE board?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The ethercat_slave project default is syncmanager + dc mode.
Have you ever configure the ethercat_slave project to FREERUN + DC mode on AM335x_ICE board?
Hi Louis,
I will ask the factory team to look at this.
Louis,
On TwinCAT, FREERUN is an asynchronous mode. Synchronization modes available are SM-Synchron and DC-Synchron.
I want to configure the ethercat stack to be FreeRun Mode(#define AL_EVENT_ENABLED 0) and DC mode (#define DC_SUPPORTED 1), but slave seems can not to trans to OP mode.
Louis,
In the stack, in comments for DC_SUPPORTED, it is mentioned that "If this switch is set, then also AL_EVENT_ENABLED shall be set." This configuration of AL_EVENT_ENABLED 0 & DC_SUPPORTED 1 will require more modifications on the stack to be run.
The EtherCAT forum might be able to provide additional support on this. http://ethercat.org
Thanks,
Srikant