Hi ,
I am working on OTG on beagleboard xm based custom board running sdk 06 version.
I want to use the vbus of OTG from a external supply to over come the internal vbus 100mA current limit,
As per http://e2e.ti.com/support/power_management/pmu/f/43/p/685/1284857.aspx#1284857 this link I need to disable the charge pump for that configuring OTG_CTRL .
I belive it cane be done from /board-support/linux-3.3.7/drivers/usb/otg/twl4030-usb.c using twl_i2c_write_u8
function .But so far it is not working !!!
can any one point me how to make the charge pump disable in ez sdk, .
ANy help is greatly appreciated.
Regards,
Dibin