Hi,
I have questions about AM437x RTC.
The question is about power supply for CAP_VDD_RTC / VDDS_RTC and
power consumption of RTC.
Q1.If using RTC functionality and RTC-only mode,
CAP_VDD_RTC doesn't need power supply but need to connect to VSS via decpoupling capacitor(1uF),
and provide 1.8V power supply to VDDS_RTC, is it correct?
Q2.If using RTC as RTC-only mode, do I need to provide power supply as following?
- CAP_VDD_RTC = 1.0V
- VDDS_RTC = 1.8V
Q3.When supplying from backup battery, what is the consumption current value required
for time measurement and time maintenance?
Q4.What is the consumption current value of RTC when the main power is ON?
I found power estimation tool, but power consumption of RTC can't be judged from the tool.
But I want to know the RTC power consumption, is there any information for Q3 and Q4?
best regards,
g.f.