Hi,
We are working with a commercial SOM that brings out all three I2C ports. We are using winCE 7.0 and have I2c0 and i2c1 working. We went to add I2c2 and have been unable to get it working. Here are some details:
1. We tested the pin muxing and HW connectivity by changing the designated I2C2 pins to GPIO pins and toggling them via SW.
2. We can read and write the virtual memory space that was created for the "I2C2" registers and have looked at the I2c2_CON register to make sure it was enabled. It was.
3. The SDA2 and SCL2 pins just remain high even when we do a I2c2 write action.
Are there any errata for the I2c2 functionality in the AM335x?
Any suggestions on things to check would be most appreciated.
Thanks,
Mitch