Hi,
There are request_irq() calls in cpsw_probe() which are setting up interrupts on pin 2,29(gpio93) and pin 2,30 (gpio94). This appears to be related to a silicon errata “Advisory 1.0.9 Ethernet Media Access Controller and Switch Subsystem: C0_TX_PEND and C0_RX_PEND Interrupts Not Connected to ARM Cortex-A8”.
However, I do not see anything connected to these pins on my AM335x board so my questions are:
1) Am I precluded from using this pins for other purposes?
2) where is the interrupt source for gpio93 and gpio92 coming from? is it the timer block?
Regards
Fergal.