Hello,
We have a custom board developed based on AM335x reference. The SYSBOOT is configured as 10011 (NAND. NANDI2C, MMC0, UART).
We are using UART0 as the console, When we power on the board with SD card having the test image (U-Boot or Diagnostic Image from TI) nothing comes in the console. Same Image works on Evaluation board EVM3358-SK-LCD.
The Baud Rate is 115200 8N1.
We have no USB port on this custom board, only UART0 is available.
Even if no SD card is inserted to the custom board, the board do not print "CCCC" .
Now to check if the board is properly working, is there any tool to detect the board for its working ??
Any Flash Tool Available for AM335x (Its AM3352) based processor. ??
Is there any mechanism to run the test program from RAM or NAND ??
Please let me know if any other mechanism.
Regards,
Sanju.