Hi,
I am accessing beaglebone black (arago linux, kernel 3.12) using ssh over ethernet.
I have noticed that if the board is turned on but no ssh connection is made after a while, I cannot connect anymore and a hardware reset must be done!
The amount of time needed to loose communication varies from some minutes to some hours.
I have already discarded supply issues! The board is supplied 5Vdc in the power jack connector.
I have tried to automatically reboot the board every 20 minutes, but it did not work!
Maybe there is something in the system putting the board to sleep or shutting it down.
Any ideas?
Thanks in advance!