Hi there! I'm trying to configure and enable watchdog in AM335x. I followed this guide: http://processors.wiki.ti.com/index.php/AM335x_PSP_WDT_Driver_User_Guide;
Anyone else noticed this issue?
[ 0.490832] console [ttyO0] enabled
[ 0.495093] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[ 0.502863] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[ 0.510671] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[ 0.518459] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[ 0.526245] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[ 0.535703] omap2_elm: probe of omap2_elm failed with error -22
[ 0.542129] omap2-nand driver initializing
[ 0.546844] ONFI flash detected
[ 0.550252] ONFI param page 0 valid
[ 0.553928] NAND device: Manufacturer ID: 0x2c, Chip ID: 0xa1 (Micron MT29F1G08ABBDAH4)
[ 0.562441] 6 cmdlinepart partitions found on MTD device omap2-nand.0
[ 0.569246] Creating 6 MTD partitions on "omap2-nand.0":
[ 0.574852] 0x000000000000-0x000000020000 : "SPL"
[ 0.581172] 0x000000020000-0x0000000a0000 : "u-boot"
[ 0.587890] 0x0000000a0000-0x000000300000 : "kernel"
[ 0.595431] 0x000000300000-0x000001c00000 : "fs"
[ 0.611888] 0x000001c00000-0x000002600000 : "drivers"
[ 0.622640] 0x000002600000-0x000008000000 : "ubi"
[ 0.666821] Unhandled fault: external abort on non-linefetch (0x1028) at 0xf9e35034
[ 0.674893] Internal error: : 1028 [#1] PREEMPT
[ 0.679655] Modules linked in:
[ 0.682873] CPU: 0 Not tainted (3.2.61.UCC3.R2 #1)
[ 0.688302] PC is at omap_wdt_disable+0xc/0x48
[ 0.692985] LR is at omap_wdt_probe+0x4a4/0x5f4
[ 0.697749] pc : [<c0183850>] lr : [<c01fd260>] psr: a0000013
[ 0.697756] sp : c302bea0 ip : 00000000 fp : c302bf04
[ 0.709824] r10: c302a000 r9 : c02ccc98 r8 : 00000000