Dear TI E2E Community,
I need to disable the Temperature sensor TCN75A in the userspace (after bootup in the shell prompt) (preventing it from reporting the temperature values in the userspace) which is interfaced to i2c0 bus, but when I see the i2cdump as shown below, the register address 0x01 contents seems to be zero but when am still able to read the temperature readings, ie., current temp of the board using sysfs
root@lifeline:/# i2cdump -f -y 0 0x48
No size specified (using byte-data access)
0 1 2 3 4 5 6 7 8 9 a b c d e f 0123456789abcdef
00: 1f 00 4b 50 XX 54 10 XX f0 95 3d 11 XX XX XX XX ?.KPXT?X??=?XXXX
10: 1e 00 4b 50 XX 54 10 XX f0 95 3d 11 XX XX XX XX ?.KPXT?X??=?XXXX
20: 1e 00 4b 50 XX 54 10 XX f0 95 3d 11 XX XX XX XX ?.KPXT?X??=?XXXX
30: 1f 00 4b 50 XX 54 10 XX f0 95 3d 11 XX XX XX XX ?.KPXT?X??=?XXXX
40: 1f 00 4b 50 XX 54 10 XX f0 95 3d 11 XX XX XX XX ?.KPXT?X??=?XXXX
50: 1f 00 4b 50 XX 54 10 XX f0 95 3d 11 XX XX XX XX ?.KPXT?X??=?XXXX
60: 1f 00 4b 50 XX 54 10 XX f0 95 3d 11 XX XX XX XX ?.KPXT?X??=?XXXX
70: 1e 00 4b 50 XX 54 10 XX f0 95 3d 11 XX XX XX XX ?.KPXT?X??=?XXXX
80: 1e 00 4b 50 XX 54 10 XX f0 95 3d 11 XX XX XX XX ?.KPXT?X??=?XXXX
90: 1e 00 4b 50 XX 54 10 XX f0 95 3d 11 XX XX XX XX ?.KPXT?X??=?XXXX
a0: 1f 00 4b 50 XX 54 10 XX f0 95 3d 11 XX XX XX XX ?.KPXT?X??=?XXXX
b0: 1f 00 4b 50 XX 54 10 XX f0 95 3d 11 XX XX XX XX ?.KPXT?X??=?XXXX
c0: 1e 00 4b 50 XX 54 10 XX f0 95 3d 11 XX XX XX XX ?.KPXT?X??=?XXXX
d0: 1e 00 4b 50 XX 54 10 XX f0 95 3d 11 XX XX XX XX ?.KPXT?X??=?XXXX
e0: 1e 00 4b 50 XX 54 10 XX f0 95 3d 11 XX XX XX XX ?.KPXT?X??=?XXXX
f0: 1f 00 4b 50 XX 54 10 XX f0 95 3d 11 XX XX XX XX ?.KPXT?X??=?XXXX
root@lifeline:/#
root@lifeline:/# cat /sys/bus/i2c/devices/0-0048/temp1_input
31000
root@lifeline:/# cat /sys/bus/i2c/devices/0-0048/temp1_input
30500
root@lifeline:/# cat /sys/bus/i2c/devices/0-0048/temp1_input
31000
root@lifeline:/# cat /sys/bus/i2c/devices/0-0048/temp1_input
Could you please let me know whether this is possible to disable temp. sensor thereby preventing it reporting the temperature values in the userspace
Kindly do the needful as early as possible
Awaiting for your replies
Many Thanks in advance