Hi, My customer are having problem with their AM437x custom board. Two 16bit DDR3L(128M) as 32bit banks are on the board. When write leveling are enabled, there are problem of write access against upper 16bit DDR3L. It can't access successfully. But it can write access against lower 16bit DDR3L successfully. They have following questions: 1. How to disable write leveling? I guess only setting '1' against EMIF4D_DDR_PHY_CTRL_1 bit[25] and EMIF4D_DDR_PHY_CTRL_1_SHADOW bit[25] will disable the write leveling of Full leveling. But I want to make me sure. Is it correct? 2. Is there any information about leveling issue for AM437x? I checked errata sheet of AM437x but there was no errata of DDR3 Leveling. best regards, g.f.