Hi
I'm using AM3354 on linux 3.2.0.
Right now i'm using gpio1_17 and gpio1_18 as an interrupt source.
but i found that the response time between the real hardware interruption and the interrupt handler i registered with kernel is entered...is really long.
normally it's at least 1ms.Sometimes it's 20ms.
this gets me into a big trouble...
How to change the interrupt of gpio1_17 and gpio1_18 to a much higher priority in linux for am3354?
thanks guys!