Hi team,
We are looking at the AM5726 and I see in the datasheet that the "Cycle time, output clock gpmc_clk period spec" (F0) is minimum 11.3 ns, which translates to about 88.5 MHz maximum. However with the AM4376, we are able to run this clock at 120 MHz.
- Is the maximum frequency on the AM5726 actually only 88.5 MHz?
- Why is this frequency lower than that of the AM4376?
Regards,
Akash Patel