Hello,
I'm interested in an extremely low-latency embedded audio solution. The AM57XX boards look awesome, but I can't seem to find any specs on the latency of the audio drivers. I've found the following table:
processors.wiki.ti.com/.../Processor_SDK_Linux_Kernel_Performance_Guide
However, I'm not sure how to deduce the latency from this, or if that information is somehow related through the table at all.
I wonder if it's possible for a dev or someone else with the same board to run an alsa loopback test similar to here:
But with rate 96kHz, frame size 96 samples, single channel, and desired latency of <= 5ms. At the highest level, I would like to see if the AM57XX is capable of < 5ms round-trip latency, and what impact it has on the CPU load. Even a general latency to CPU load measurement is fine enough to get started.
I would also be interested on this might theoretically change, or actually will change with an RTOS, or if there are alternative solutions such as grabbing PCM data before it hits the ARM similar to Snapdragon platforms, etc (I'm not extremely familiar with the AM57X architecture at this point.
Sorry for the extremely general question. This platform looks really amazing, but I just need a little more information.