Other Parts Discussed in Thread: AM5718
Hi,
Could you tell me the Adjusted Peak Performance (APP) of AM5728?
Best regards,
H.U
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Here is the quick math for AM5728 APP value
A15 does 1 DP FMAC instruction (FMAC is 2 FLOPS, multiply and add) in 1 cycle, so peak floating point capability (Ri) is 2. It is not vector (with 64b floats) so Wi is 0.3.
C66x does 4 DP float operations per cycle, Ri is 4. Not vectors as defined by export control for DP floats, Wi is 0.3.
Multiply with clock and the number of cores the answer in Tera.
A15's is 2*0.3*1.5G is 0.0009 Weighted TeraFLOPS C66x's is 4*0.3*0.75G is 0.0009 Weighted TeraFLOPS
AM5728 is 0.0018 Weighted TeraFLOPS
You can refer to page 6 "Technical Notes On Adjusted Peak Peformance" on additional background and notes
Regards
Mukul
Hi Mukul,
Thank you for your reply.
AM5728 have two A15 core and two C66x core, so I think AM5728 is 0.0072 Weighted TeraFLOPS. right?
Best regards,
H.U