Hi,
Are the Phy address on the PRU MDIO preset in the PRU-ICSS-HSR-PRP firmware? Can the MDIO addresses be changed?
Do to the limitation of the 3rd party SOM we are using we will have 3 Phys connected to the PRU MDIO (2 to PRU MII and one to RGMII). We are aware that we won't be able to use the MDIO for configuring the Phy on RGMII it will be configured via bootstrap pins. Can this setup work or will the 3rd Phy interfere withe the firmware on the PRU?