Other Parts Discussed in Thread: AM3358
Tool/software: Linux
Hello there,
We have a custom board using AM3352 processor, we are in a board bring up state of the project. Our custom board is based on the Beaglebone Green Wireless device, and I have compiled the latest Arago images for the project using processor-sdk-04.00.00.04. I compiled the entire tisdk using arago-core-tisdk-image. After the successful compilation I have list of images in my Build deploy directory. Listed below are the few I wanted to use to boot my custom board.
-
MLO-am335x-evm-2017.01+gitAUTOINC+9fd60700db-r4 ----> MLO
-
u-boot-am335x-evm-2017.01+gitAUTOINC+9fd60700db-r4.img ----> u-boot.img
-
zImage--4.9.28+git0+eed43d1050-r22c.arago5.tisdk3-am335x-bonegreen-20170912170513.dtb
-
zImage--4.9.28+git0+eed43d1050-r22c.arago5.tisdk3-am335x-evm-20170912170513.bin ----> zImage
-
tisdk-rootfs-image-am335x-evm-20170914131632.rootfs.tar.xz
I have changed name of all the files appropriately.
First of all, I want to boot the images (at least MLO and u-boot) from the SD Card, and to create a compatible SD Card I have used following technique.
After I created the SD Card, I put MLO, u-boot.img and other files on it and inserted to the custom board. I made sure that SYSBOOT are configured in a way it can boot from SD Card.
MAIN ISSUE:
The problem is, when I insert the SD card and turn on the board, it does not show anything on the console. Without SD card inserted I can see ROM code trying UART boot with "CCCCCCCCCCCCCCCCCCC.." on console.
I also have beaglebone Green Wireless and it's SD card .img file. If I try to boot beaglebone Green Wireless using the same SD card, it does boot properly through SD card and I can see the Arago Project console login shell.
If I burn the Beaglebone Green Wireless' .img file to an SD card and insert it to my custom board, my custom board does boot from the SD card and complete till kernel booting.
SAME THING IS HAPPENING FOR BEAGLEBONE BLACK is well.
QUE. :
Since, Beaglebone Green Wireless has AM3358, does that make a difference in booting process?
What is the possible cause of this issue?
What is the ideal SD card booting process for AM3352?
Thank you,
Divyeshkumar