Tool/software: Linux
Hi all,
My question is how to set the boot state of GPIO,I tried to change the GPIO state modifying the muxdata.h file in u-boot path,however,it didn't works,I modify the VOUT1_D6 in M14 as GPIO8_6 and pull up to output,but when i boot my board,the status of GPIO8_6 is still lo,the other configuration of the muxdata.h file actually works like the pinmux of VIN3a or uart.
Could u give me some insight on how to set the state of GPIO when the board is start?Which file should i modify?Following is my muxdata.h file.