Tool/software: Linux
Dear Sirs,
I have 2 projects using AM3352. Both are based on BeagleBone Black schematics. One is with 10/100 Ethernet phy and the other is with Realtek RTL8211E Gigabit phy. The 10/100 board works fine. The other board is based on RTL8211E 10/100/1000 Phy cannot work, please see attached log file.
Attached log file showed that I have done some tests, please review the log file to see if there is something abnormal.
When booting up Ubuntu, it will take 5 minutes and finally got "Failed to start Raise network interfaces." error message.
We only need one Ethernet which connected to RGMII1 (CPSW slave 1) of AM335x. The phy_addr is set at 01.
When we ping, if the LAN cable is connected, we got "Destination Host Unreachable" error, if we unplug the cable, we got "ping: sendmsg: Network is unreachable" error instead.
We have measured the RGMII_RXCLK and RGMII_TXCLK with a scope, we saw steady 125MHz clock on both pins. Does it mean the RGMII mode was already set correctly?
Since we have ported 10/100 Ethernet port correctly, we reverse compiled their dtb files to dts files then compared with gigabit's dts files the diff utility, please see log file. We feel that
U-Boot 2018.03-dirty (Aug 11 2018 - 06:12:21 -0700) CPU : AM335X-GP rev 2.1 I2C: ready DRAM: 512 MiB No match for driver 'omap_hsmmc' No match for driver 'omap_hsmmc' Some drivers were not found Reset Source: Global external warm reset has occurred. Reset Source: Power-on reset has occurred. RTC 32KCLK Source: External. MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 Loading Environment from EXT4... OK Board: BeagleBone Black BeagleBone Black: BeagleBone: cape eeprom: i2c_probe: 0x54: BeagleBone: cape eeprom: i2c_probe: 0x55: BeagleBone: cape eeprom: i2c_probe: 0x56: BeagleBone: cape eeprom: i2c_probe: 0x57: Net: eth0: UDS RGMII MODE cpsw, usb_ether Press SPACE to abort autoboot in 2 seconds board_name=[A335BNLT] ... board_rev=[] ... switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 ** Bad device 0:2 0x82000000 ** ** Bad device 0:2 0x82000000 ** switch to partitions #0, OK mmc0 is current device Scanning mmc 0:1... gpio: pin 56 (gpio 56) value is 0 gpio: pin 55 (gpio 55) value is 0 gpio: pin 54 (gpio 54) value is 0 gpio: pin 53 (gpio 53) value is 1 switch to partitions #0, OK mmc0 is current device gpio: pin 54 (gpio 54) value is 1 Checking for: /uEnv.txt ... Checking for: /boot.scr ... Checking for: /boot/boot.scr ... Checking for: /boot/uEnv.txt ... gpio: pin 55 (gpio 55) value is 1 46 bytes read in 32 ms (1000 Bytes/s) Loaded environment from /boot/uEnv.txt Checking if uname_r is set in /boot/uEnv.txt... gpio: pin 56 (gpio 56) value is 1 Running uname_boot ... loading /boot/vmlinuz-4.14.41-bone14 ... 10387968 bytes read in 689 ms (14.4 MiB/s) loading /boot/dtbs/4.14.41-bone14/am335x-boneblack.dtb ... 60811 bytes read in 101 ms (587.9 KiB/s) uboot_overlays: add [enable_uboot_overlays=1] to /boot/uEnv.txt to enable... debug: [console=ttyO0,115200n8 root=/dev/mmcblk0p1 ro rootfstype=ext4 rootwait] ... debug: [bootz 0x82000000 - 0x88000000] ... ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 8ffee000, end 8ffffd8a ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 4.14.41-bone14 (root@ubuntu) (gcc version 7.2.1 20171011 (Linaro GCC 7.2-2017.11)) #1 PREEMPT Thu Aug 9 10:08:07 PDT 2018 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] OF: fdt: Machine model: TI AM335x BeagleBone Black [ 0.000000] Memory policy: Data cache writeback [ 0.000000] efi: Getting EFI parameters from FDT: [ 0.000000] efi: UEFI not found. [ 0.000000] cma: Reserved 48 MiB at 0x9d000000 [ 0.000000] CPU: All CPU(s) started in SVC mode. [ 0.000000] AM335X ES2.1 (neon) [ 0.000000] random: get_random_bytes called from start_kernel+0xac/0x44c with crng_init=0 [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 129920 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p1 ro rootfstype=ext4 rootwait [ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes) [ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes) [ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Memory: 447468K/524288K available (13312K kernel code, 1125K rwdata, 4204K rodata, 1024K init, 634K bss, 27668K reserved, 49152K cma-reserved, 0K highmem) [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB) [ 0.000000] vmalloc : 0xe0800000 - 0xff800000 ( 496 MB) [ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB) [ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB) [ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB) [ 0.000000] .text : 0xc0008000 - 0xc0e00000 (14304 kB) [ 0.000000] .init : 0xc1400000 - 0xc1500000 (1024 kB) [ 0.000000] .data : 0xc1500000 - 0xc1619514 (1126 kB) [ 0.000000] .bss : 0xc1623340 - 0xc16c1b94 ( 635 kB) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1 [ 0.000000] ftrace: allocating 41784 entries in 123 pages [ 0.000000] Preemptible hierarchical RCU implementation. [ 0.000000] Tasks RCU enabled. [ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16 [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts [ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz [ 0.000016] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns [ 0.000036] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns [ 0.000047] OMAP clocksource: timer1 at 24000000 Hz [ 0.000505] timer_probe: no matching timers found [ 0.000703] Console: colour dummy device 80x30 [ 0.000727] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0' [ 0.000734] This ensures that you still see kernel messages. Please [ 0.000739] update your kernel commandline. [ 0.000760] Calibrating delay loop... 995.32 BogoMIPS (lpj=1990656) [ 0.047025] pid_max: default: 32768 minimum: 301 [ 0.047283] Security Framework initialized [ 0.047301] Yama: becoming mindful. [ 0.047385] AppArmor: AppArmor initialized [ 0.047594] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.047608] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.048498] CPU: Testing write buffer coherency: ok [ 0.049314] Setting up static identity map for 0x80100000 - 0x80100060 [ 0.049475] Hierarchical SRCU implementation. [ 0.052418] EFI services will not be available. [ 0.053894] devtmpfs: initialized [ 0.065693] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 0.066070] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.066093] futex hash table entries: 256 (order: -1, 3072 bytes) [ 0.069939] xor: measuring software checksum speed [ 0.107094] arm4regs : 1219.000 MB/sec [ 0.147032] 8regs : 957.000 MB/sec [ 0.187022] 32regs : 1053.000 MB/sec [ 0.227020] neon : 1642.000 MB/sec [ 0.227028] xor: using function: neon (1642.000 MB/sec) [ 0.227049] pinctrl core: initialized pinctrl subsystem [ 0.227742] DMI not present or invalid. [ 0.228142] NET: Registered protocol family 16 [ 0.230537] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 0.247553] omap_hwmod: debugss: _wait_target_disable failed [ 0.287784] cpuidle: using governor menu [ 0.292236] OMAP GPIO hardware version 0.1 [ 0.302592] No ATAGs? [ 0.302611] hw-breakpoint: debug architecture 0x4 unsupported. [ 0.379168] raid6: neonx2 gen() 1896 MB/s [ 0.447049] raid6: neonx2 xor() 1525 MB/s [ 0.447060] raid6: using algorithm neonx2 gen() 1896 MB/s [ 0.447068] raid6: .... xor() 1525 MB/s, rmw enabled [ 0.447076] raid6: using neon recovery algorithm [ 0.453025] edma 49000000.edma: TI EDMA DMA engine driver [ 0.455095] SCSI subsystem initialized [ 0.455719] usbcore: registered new interface driver usbfs [ 0.455774] usbcore: registered new interface driver hub [ 0.455875] usbcore: registered new device driver usb [ 0.456351] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring probe [ 0.457542] omap_i2c 4819c000.i2c: bus 2 rev0.11 at 100 kHz [ 0.457789] media: Linux media interface: v0.10 [ 0.457837] Linux video capture interface: v2.00 [ 0.457893] pps_core: LinuxPPS API ver. 1 registered [ 0.457901] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 0.457921] PTP clock support registered [ 0.458047] dmi: Firmware registration failed. [ 0.458416] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400 [ 0.459129] Advanced Linux Sound Architecture Driver Initialized. [ 0.460328] NetLabel: Initializing [ 0.460345] NetLabel: domain hash size = 128 [ 0.460352] NetLabel: protocols = UNLABELED CIPSOv4 CALIPSO [ 0.460437] NetLabel: unlabeled traffic allowed by default [ 0.461103] clocksource: Switched to clocksource timer1 [ 0.596966] VFS: Disk quotas dquot_6.6.0 [ 0.597065] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) [ 0.597731] AppArmor: AppArmor Filesystem Enabled [ 0.607260] NET: Registered protocol family 2 [ 0.608048] TCP established hash table entries: 4096 (order: 2, 16384 bytes) [ 0.608096] TCP bind hash table entries: 4096 (order: 2, 16384 bytes) [ 0.608136] TCP: Hash tables configured (established 4096 bind 4096) [ 0.608241] UDP hash table entries: 256 (order: 0, 4096 bytes) [ 0.608260] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) [ 0.608438] NET: Registered protocol family 1 [ 0.609053] RPC: Registered named UNIX socket transport module. [ 0.609070] RPC: Registered udp transport module. [ 0.609076] RPC: Registered tcp transport module. [ 0.609083] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.610164] hw perfevents: no interrupt-affinity property for /pmu, guessing. [ 0.610275] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available [ 0.612453] audit: initializing netlink subsys (disabled) [ 0.613261] audit: type=2000 audit(0.608:1): state=initialized audit_enabled=0 res=1 [ 0.613759] workingset: timestamp_bits=14 max_order=17 bucket_order=3 [ 0.618617] zbud: loaded [ 0.621056] NFS: Registering the id_resolver key type [ 0.621248] Key type id_resolver registered [ 0.621261] Key type id_legacy registered [ 0.621283] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 0.621609] fuse init (API version 7.26) [ 0.622391] orangefs_debugfs_init: called with debug mask: :none: :0: [ 0.622564] orangefs_init: module version upstream loaded [ 0.622575] SGI XFS with ACLs, security attributes, realtime, no debug enabled [ 0.631281] Key type asymmetric registered [ 0.631305] Asymmetric key parser 'x509' registered [ 0.631418] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245) [ 0.631661] io scheduler noop registered [ 0.631674] io scheduler deadline registered [ 0.631990] io scheduler cfq registered (default) [ 0.632000] io scheduler mq-deadline registered [ 0.633300] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568 [ 0.634285] gpio-of-helper ocp:cape-universal: ready [ 0.636118] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle [ 0.637575] Serial: 8250/16550 driver, 6 ports, IRQ sharing disabled [ 0.640469] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 30, base_baud = 3000000) is a 8250 [ 1.234581] random: fast init done [ 1.431442] console [ttyS0] enabled [ 1.437326] omap_rng 48310000.rng: Random Number Generator ver. 20 [ 1.444491] [drm] Initialized vgem 1.0.0 20120112 for virtual device on minor 0 [ 1.452057] usbcore: registered new interface driver udl [ 1.459729] at24 2-0054: 32768 byte 24c256 EEPROM, writable, 1 bytes/write [ 1.467036] at24 2-0055: 32768 byte 24c256 EEPROM, writable, 1 bytes/write [ 1.474187] at24 2-0056: 32768 byte 24c256 EEPROM, writable, 1 bytes/write [ 1.481316] at24 2-0057: 32768 byte 24c256 EEPROM, writable, 1 bytes/write [ 1.490762] libphy: Fixed MDIO Bus: probed [ 1.495788] CAN device driver interface [ 1.553197] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000 [ 1.560930] davinci_mdio 4a101000.mdio: detected phy mask fffffffc [ 1.569882] libphy: 4a101000.mdio: probed [ 1.574031] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver RTL8211E Gigabit Ethernet [ 1.583736] davinci_mdio 4a101000.mdio: phy[1]: device 4a101000.mdio:01, driver RTL8211E Gigabit Ethernet [ 1.594208] cpsw 4a100000.ethernet: Detected MACID = 90:70:65:c4:80:22 [ 1.601028] cpsw 4a100000.ethernet: cpts: overflow check period 1250 (jiffies) [ 1.609853] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver [ 1.616516] ehci-platform: EHCI generic platform driver [ 1.621960] ehci-omap: OMAP-EHCI Host Controller driver [ 1.627436] usbcore: registered new interface driver usb-storage [ 1.635458] am335x-phy-driver 47401300.usb-phy: 47401300.usb-phy supply vcc not found, using dummy regulator [ 1.647592] am335x-phy-driver 47401b00.usb-phy: 47401b00.usb-phy supply vcc not found, using dummy regulator [ 1.669050] omap_rtc 44e3e000.rtc: already running [ 1.674522] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc0 [ 1.682537] i2c /dev entries driver [ 1.688195] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 1.695566] softdog: initialized. soft_noboot=0 soft_margin=60 sec soft_panic=0 (nowayout=1) [ 1.705413] omap_hsmmc 48060000.mmc: Got CD GPIO [ 1.784333] mmc0: host does not support reading read-only switch, assuming write-enable [ 1.793777] ledtrig-cpu: registered to indicate activity on CPUs [ 1.794115] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2 [ 1.800460] omap-aes 53500000.aes: will run requests pump with realtime priority [ 1.807881] omap-sham 53100000.sham: hw accel on OMAP rev 4.3 [ 1.822825] hidraw: raw HID events driver (C) Jiri Kosina [ 1.823349] usbcore: registered new interface driver usbhid [ 1.823353] usbhid: USB HID core driver [ 1.823673] remoteproc remoteproc0: wkup_m3 is available [ 1.827469] wireguard: WireGuard 0.0.20180514 loaded. See www.wireguard.com for information. [ 1.827476] wireguard: Copyright (C) 2015-2018 Jason A. Donenfeld <Jason@zx2c4.com>. All Rights Reserved. [ 1.828207] NET: Registered protocol family 10 [ 1.835353] Segment Routing with IPv6 [ 1.835425] mip6: Mobile IPv6 [ 1.835439] NET: Registered protocol family 17 [ 1.835453] can: controller area network core (rev 20170425 abi 9) [ 1.835535] NET: Registered protocol family 29 [ 1.835624] Key type dns_resolver registered [ 1.835628] mpls_gso: MPLS GSO support [ 1.835815] omap_voltage_late_init: Voltage driver support not added [ 1.835830] ThumbEE CPU extension supported. [ 1.835844] Registering SWP/SWPB emulation handler [ 1.836651] registered taskstats version 1 [ 1.836773] zswap: loaded using pool lzo/zbud [ 1.839120] Btrfs loaded, crc32c=crc32c-generic [ 1.839215] AppArmor: AppArmor sha1 policy hashing enabled [ 1.839232] ima: No TPM chip found, activating TPM-bypass! (rc=-19) [ 1.953683] mmc0: new high speed SDHC card at address 0007 [ 1.963051] mmcblk0: mmc0:0007 SD16G 14.4 GiB [ 1.969509] mmcblk0: p1 [ 1.996306] input: tps65217_pwr_but as /devices/platform/ocp/44e0b000.i2c/i2c-0/0-0024/tps65217-pwrbutton/input/input0 [ 2.007768] tps65217 0-0024: TPS65217 ID 0xe version 1.2 [ 2.013652] at24 0-0050: 32768 byte 24c256 EEPROM, writable, 1 bytes/write [ 2.022206] tda998x 0-0070: Error -121 writing to cec:0xff [ 2.027928] tda998x 0-0070: set_page 000a err -121 [ 2.032875] mmc1: new high speed MMC card at address 0001 [ 2.038965] mmcblk1: mmc1:0001 M62704 1.77 GiB [ 2.043815] mmcblk1boot0: mmc1:0001 M62704 partition 1 2.00 MiB [ 2.050026] mmcblk1boot1: mmc1:0001 M62704 partition 2 2.00 MiB [ 2.056188] mmcblk1rpmb: mmc1:0001 M62704 partition 3 512 KiB [ 2.089213] tda998x 0-0070: set_page 000a err -121 [ 2.153173] tda998x 0-0070: set_page 0001 err -121 [ 2.158065] tda998x 0-0070: set_page 0001 err -121 [ 2.162948] tda998x 0-0070: set_page 0200 err -121 [ 2.167856] tda998x 0-0070: set_page 0201 err -121 [ 2.172745] tda998x 0-0070: set_page 0202 err -121 [ 2.177630] tda998x 0-0070: set_page 0203 err -121 [ 2.182516] tda998x 0-0070: set_page 0204 err -121 [ 2.187402] tda998x 0-0070: set_page 0205 err -121 [ 2.192281] tda998x 0-0070: set_page 020e err -121 [ 2.197171] tda998x 0-0070: set_page 0211 err -121 [ 2.202056] tda998x 0-0070: set_page 0207 err -121 [ 2.206940] tda998x 0-0070: set_page 0208 err -121 [ 2.211824] tda998x 0-0070: set_page 0209 err -121 [ 2.216710] tda998x 0-0070: set_page 020a err -121 [ 2.221594] tda998x 0-0070: set_page 0206 err -121 [ 2.226479] tda998x 0-0070: set_page 0027 err -121 [ 2.231363] tda998x 0-0070: set_page 0000 err -121 [ 2.236247] tda998x 0-0070: set_page 0002 err -121 [ 2.241288] tilcdc 4830e000.lcdc: failed to bind 0-0070 (ops tda998x_ops): -6 [ 2.248713] tilcdc 4830e000.lcdc: master bind failed: -6 [ 2.254381] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz [ 2.261394] remoteproc remoteproc0: powering up wkup_m3 [ 2.266792] remoteproc remoteproc0: Booting fw image am335x-pm-firmware.elf, size 217168 [ 2.275239] remoteproc remoteproc0: remote processor wkup_m3 is now up [ 2.281807] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x193 [ 2.291866] bone_capemgr bone_capemgr: Baseboard: 'A335BNLT,����,������������' [ 2.299188] bone_capemgr bone_capemgr: compatible-baseboard=ti,beaglebone-black - #slots=4 [ 2.334074] bone_capemgr bone_capemgr: slot #0: No cape found [ 2.366235] bone_capemgr bone_capemgr: slot #1: No cape found [ 2.398387] bone_capemgr bone_capemgr: slot #2: No cape found [ 2.430538] bone_capemgr bone_capemgr: slot #3: No cape found [ 2.436382] bone_capemgr bone_capemgr: initialized OK. [ 2.451101] musb-hdrc musb-hdrc.1: MUSB HDRC host driver [ 2.456517] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1 [ 2.464222] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 [ 2.471075] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 2.478345] usb usb1: Product: MUSB HDRC host driver [ 2.483347] usb usb1: Manufacturer: Linux 4.14.41-bone14 musb-hcd [ 2.489481] usb usb1: SerialNumber: musb-hdrc.1 [ 2.494749] hub 1-0:1.0: USB hub found [ 2.498671] hub 1-0:1.0: 1 port detected [ 2.504469] cpufreq: cpufreq_online: CPU0: Running at unlisted freq: 1000000 KHz [ 2.512066] cpu cpu0: dev_pm_opp_set_rate: failed to find current OPP for freq 1000000000 (-34) [ 2.522907] cpufreq: cpufreq_online: CPU0: Unlisted initial frequency changed to: 600000 KHz [ 2.533343] omap_rtc 44e3e000.rtc: setting system clock to 2000-01-01 00:02:35 UTC (946684955) [ 2.542107] of_cfs_init [ 2.544717] of_cfs_init: OK [ 2.548424] ALSA device list: [ 2.551497] No soundcards found. [ 2.559449] EXT4-fs (mmcblk0p1): INFO: recovery required on readonly filesystem [ 2.566981] EXT4-fs (mmcblk0p1): write access will be enabled during recovery [ 2.700722] EXT4-fs (mmcblk0p1): recovery complete [ 2.710715] EXT4-fs (mmcblk0p1): mounted filesystem with ordered data mode. Opts: (null) [ 2.719039] VFS: Mounted root (ext4 filesystem) readonly on device 179:1. [ 2.729331] devtmpfs: mounted [ 2.737649] Freeing unused kernel memory: 1024K [ 2.965189] usb 1-1: new high-speed USB device number 2 using musb-hdrc [ 3.052638] systemd[1]: System time before build time, advancing clock. [ 3.122859] usb 1-1: New USB device found, idVendor=05e3, idProduct=0610 [ 3.137262] usb 1-1: New USB device strings: Mfr=0, Product=1, SerialNumber=0 [ 3.149350] usb 1-1: Product: USB2.0 Hub [ 3.156019] hub 1-1:1.0: USB hub found [ 3.160992] hub 1-1:1.0: 4 ports detected [ 3.187028] random: systemd: uninitialized urandom read (16 bytes read) [ 3.198088] random: systemd: uninitialized urandom read (16 bytes read) [ 3.222568] systemd[1]: systemd 229 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +ACL +XZ -LZ4 +SECCOMP +BLKID +ELFUTILS +KMOD -IDN) [ 3.241953] systemd[1]: Detected architecture arm. Welcome to [1mUbuntu 16.04.3 LTS[0m! [ 3.263012] systemd[1]: Set hostname to <arm>. [ 3.432015] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read) [ 3.457358] usb 1-1.2: new high-speed USB device number 3 using musb-hdrc [ 3.557743] usb 1-1.2: New USB device found, idVendor=1a40, idProduct=0201 [ 3.565252] usb 1-1.2: New USB device strings: Mfr=0, Product=1, SerialNumber=0 [ 3.577335] usb 1-1.2: Product: USB 2.0 Hub [MTT] [ 3.584652] hub 1-1.2:1.0: USB hub found [ 3.589464] hub 1-1.2:1.0: 7 ports detected [ 3.881277] usb 1-1.2.2: new high-speed USB device number 4 using musb-hdrc [ 3.989736] usb 1-1.2.2: New USB device found, idVendor=1a40, idProduct=0201 [ 4.005310] usb 1-1.2.2: New USB device strings: Mfr=0, Product=1, SerialNumber=0 [ 4.014336] systemd[1]: Reached target Encrypted Volumes. [[0;32m OK [0m] Reached target Encrypted Volumes. [ 4.021247] usb 1-1.2.2: Product: USB 2.0 Hub [MTT] [ 4.031865] hub 1-1.2.2:1.0: USB hub found [ 4.037036] systemd[1]: Started Dispatch Password Requests to Console Directory Watch. [[0;32m OK [0m] Started Dispatch Password Requests to Console[ 4.045857] hub 1-1.2.2:1.0: 7 ports detected Directory Watch. [ 4.066183] systemd[1]: Listening on udev Control Socket. [[0;32m OK [0m] Listening on udev Control Socket. [ 4.081764] systemd[1]: Listening on fsck to fsckd communication Socket. [[0;32m OK [0m] Listening on fsck to fsckd communication Socket. [ 4.105949] systemd[1]: Started Forward Password Requests to Wall Directory Watch. [[0;32m OK [0m] Started Forward Password Requests to Wall Directory Watch. [ 4.130132] systemd[1]: Listening on Journal Audit Socket. [[0;32m OK [0m] Listening on Journal Audit Socket. [ 4.137188] usb 1-1.2.4: new high-speed USB device number 5 using musb-hdrc [ 4.148865] systemd[1]: Started Trigger resolvconf update for networkd DNS. [[0;32m OK [0m] Started Trigger resolvconf update for networkd DNS. [[0;32m OK [0m] Reached target Paths. [[0;32m OK [0m] Reached target Swap. [[0;32m OK [0m] Listening on Journal Socket. [[0;32m OK [0m] Reached target Remote File Systems (Pre). [[0;32m OK [0m] Reached target Remote File Systems. [[0;32m OK [0m] Set up automount Arbitrary Executab...ats File System Automount Point. [[0;32m OK [0m] Listening on /dev/initctl Compatibility Named Pipe. [[0;32m OK [0m] Listening on udev Kernel Socket. [ 4.274608] usb 1-1.2.4: New USB device found, idVendor=0951, idProduct=16ae [[0;32m OK [0m] Created slice System Slice. [ 4.283896] usb 1-1.2.4: New USB device strings: Mfr=1, Product=2, SerialNumber=3 [ 4.297391] usb 1-1.2.4: Product: DT microDuo 3C [ 4.303370] usb 1-1.2.4: Manufacturer: Kingston [ 4.308649] usb 1-1.2.4: SerialNumber: 94DE8072478CB1B02962A974 [ 4.322587] usb-storage 1-1.2.4:1.0: USB Mass Storage device detected Starting Load Kernel Modules... [ 4.341547] alloc_contig_range: [9d042, 9d043) PFNs busy [ 4.357311] usb 1-1.2.2.1: new full-speed USB device number 6 using musb-hdrc [ 4.386416] scsi host0: usb-storage 1-1.2.4:1.0 Starting File System Check on Root Device... [[0;32m OK [0m] Created slice system-serial\x2dgetty.slice. Mounting Debug File System... Starting Set console keymap... [ 4.483892] usb 1-1.2.2.1: New USB device found, idVendor=0403, idProduct=6001 [ 4.497807] usb 1-1.2.2.1: New USB device strings: Mfr=1, Product=2, SerialNumber=3 [ 4.522045] usb 1-1.2.2.1: Product: FT232R USB UART [ 4.522057] usb 1-1.2.2.1: Manufacturer: FTDI [ 4.522066] usb 1-1.2.2.1: SerialNumber: A9074NKH Starting Nameserver information manager... [[0;32m OK [0m] Listening on Syslog Socket. [ 4.637377] usb 1-1.2.2.2: new full-speed USB device number 7 using musb-hdrc Starting Create list of required st... nodes for the current kernel... [[0;32m OK [0m] Created slice User and Session Slice. [[0;32m OK [0m] Reached target Slices. [[0;32m OK [0m] Listening on Journal Socket (/dev/log). Starting Journal Service... [ 4.783922] usb 1-1.2.2.2: New USB device found, idVendor=0403, idProduct=6001 [ 4.821543] usb 1-1.2.2.2: New USB device strings: Mfr=1, Product=2, SerialNumber=3 [ 4.821555] usb 1-1.2.2.2: Product: FT232R USB UART [ 4.821564] usb 1-1.2.2.2: Manufacturer: FTDI [ 4.821572] usb 1-1.2.2.2: SerialNumber: A9074NKJ [ 4.929328] usb 1-1.2.2.3: new full-speed USB device number 8 using musb-hdrc Mounting POSIX Message Queue File System... [ 5.055317] usb 1-1.2.2.3: New USB device found, idVendor=0403, idProduct=6001 [ 5.077298] usb 1-1.2.2.3: New USB device strings: Mfr=1, Product=2, SerialNumber=3 [[0;32m OK [0m] Mounted Debug File System. [ 5.105846] usb 1-1.2.2.3: Product: FT232R USB UART [[0;32m OK [0m] Mounted POSIX Message Queue File System. [ 5.133737] usb 1-1.2.2.3: Manufacturer: FTDI [[0;32m OK [0m] Started Load Kernel Modules. [ 5.165746] usb 1-1.2.2.3: SerialNumber: A9074NKM [[0;32m OK [0m] Started File System Check on Root Device. [[0;32m OK [0m] Started Create list of required sta...ce nodes for the current kernel. [ 5.305335] usb 1-1.2.2.4: new full-speed USB device number 9 using musb-hdrc [[0;32m OK [0m[ 5.410670] scsi 0:0:0:0: Direct-Access Kingston DT microDuo 3C PMAP PQ: 0 ANSI: 6 ] Started Nameserver information manager. [ 5.446829] usb 1-1.2.2.4: New USB device found, idVendor=0403, idProduct=6001 [ 5.470166] sd 0:0:0:0: [sda] 60555264 512-byte logical blocks: (31.0 GB/28.9 GiB) [ 5.470573] sd 0:0:0:0: [sda] Write Protect is off [ 5.470959] sd 0:0:0:0: [sda] Write cache: disabled, read cache: enabled, doesn't support DPO or FUA [ 5.549921] usb 1-1.2.2.4: New USB device strings: Mfr=1, Product=2, SerialNumber=3 [ 5.576300] usb 1-1.2.2.4: Product: FT232R USB UART [ 5.589439] usb 1-1.2.2.4: Manufacturer: FTDI [ 5.605344] usb 1-1.2.2.4: SerialNumber: A9074NKN [ 5.610802] sda: sda1 [ 5.613737] sd 0:0:0:0: [sda] Attached SCSI removable disk [[0;32m OK [0m] Started Set console keymap. [ 5.753272] usb 1-1.2.2.5: new full-speed USB device number 10 using musb-hdrc [ 5.899632] usb 1-1.2.2.5: New USB device found, idVendor=0403, idProduct=6001 [ 5.921410] usb 1-1.2.2.5: New USB device strings: Mfr=1, Product=2, SerialNumber=3 [ 5.952729] usb 1-1.2.2.5: Product: FT232R USB UART [ 5.952741] usb 1-1.2.2.5: Manufacturer: FTDI [ 5.952749] usb 1-1.2.2.5: SerialNumber: A9074NKL [[0;32m OK [0m] Started Journal Service. [ 6.065298] usb 1-1.2.2.6: new full-speed USB device number 11 using musb-hdrc [ 6.211556] usb 1-1.2.2.6: New USB device found, idVendor=0403, idProduct=6001 [ 6.230569] usb 1-1.2.2.6: New USB device strings: Mfr=1, Product=2, SerialNumber=3 [ 6.261306] usb 1-1.2.2.6: Product: FT232R USB UART [ 6.281416] usb 1-1.2.2.6: Manufacturer: FTDI [ 6.292860] usb 1-1.2.2.6: SerialNumber: A9074NKK [ 6.393400] usb 1-1.2.2.7: new high-speed USB device number 12 using musb-hdrc [ 6.518266] usb 1-1.2.2.7: New USB device found, idVendor=1a40, idProduct=0201 [ 6.533398] usb 1-1.2.2.7: New USB device strings: Mfr=0, Product=1, SerialNumber=0 [ 6.549245] usb 1-1.2.2.7: Product: USB 2.0 Hub [MTT] [ 6.562430] hub 1-1.2.2.7:1.0: USB hub found [ 6.573510] hub 1-1.2.2.7:1.0: 7 ports detected [[0;32m OK [0m] Reached target Network (Pre). [[0;32m OK [0m] Started File System Check Daemon to report status. Starting Create Static Device Nodes in /dev... Starting Remount Root and Kernel File Systems... Starting Apply Kernel Variables... Mounting FUSE Control File System... [ 6.812702] EXT4-fs (mmcblk0p1): re-mounted. Opts: errors=remount-ro Mounting Configuration File System... [[0;32m OK [0m] Mounted FUSE Control File System. [[0;32m OK [0m] Mounted Configuration File System. [[0;32m OK [0m] Started Create Static Device Nodes in /dev. [[0;32m OK [0m] Started Remount Root and Kernel File Systems. [[0;32m OK [0m] Started Apply Kernel Variables. Starting Load/Save Random Seed... Starting Flush Journal to Persistent Storage... Starting udev Coldplug all Devices... [[0;32m OK [0m] Reached target Local File Systems (Pre). [[0;32m OK [0m] Reached target Local File Systems. Starting Raise network interfaces... Starting Set console font and keymap... Starting udev Kernel Device Manager... [[0;32m OK [0m] Started Load/Save Random Seed. [[0;32m OK [0m] Started Flush Journal to Persistent Storage. [[0;32m OK [0m] Started udev Kernel Device Manager. Starting Create Volatile Files and Directories... [[0;32m OK [0m] Started Create Volatile Files and Directories. Starting Update UTMP about System Boot/Shutdown... Starting Network Time Synchronization... [[0;32m OK [0m] Started Network Time Synchronization. [[0;32m OK [0m] Started Update UTMP about System Boot/Shutdown. [[0;32m OK [0m] Reached target System Time Synchronized. [[0;32m OK [0m] Started Set console font and keymap. [[0;32m OK [0m] Created slice system-getty.slice. [[0;32m OK [0m] Started udev Coldplug all Devices. [[0;32m OK [0m] Reached target System Initialization. [[0;32m OK [0m] Listening on Avahi mDNS/DNS-SD Stack Activation Socket. [[0;32m OK [0m] Started Daily Cleanup of Temporary Directories. [[0;32m OK [0m] Listening on D-Bus System Message Bus Socket. [[0;32m OK [0m] Reached target Sockets. [[0;32m OK [0m] Reached target Basic System. Starting LSB: Load kernel modules needed to enable cpufreq scaling... Starting System Logging Service... Starting Login Service... Starting Connection service... [[0;32m OK [0m] Started D-Bus System Message Bus. [[0;32m OK [0m] Started Connection service. Starting LSB: Set the CPU Frequency Scaling governor to "ondemand"... [[0;32m OK [0m] Started Regular background program processing daemon. Starting oFono Mobile telephony stack... Starting LSB: Start busybox udhcpd at boot time... Starting Cape Manager Service... Starting Avahi mDNS/DNS-SD Stack... Starting Permit User Sessions... Starting Generic Board Startup... [[0;32m OK [0m] Started System Logging Service. [[0;32m OK [0m] Started Cape Manager Service. [[0;32m OK [0m] Started Permit User Sessions. [[0;32m OK [0m] Started LSB: Set the CPU Frequency Scaling governor to "ondemand". [[0;32m OK [0m] Started LSB: Start busybox udhcpd at boot time. [[0;32m OK [0m] Started oFono Mobile telephony stack. [[0;32m OK [0m] Started Avahi mDNS/DNS-SD Stack. [[0;32m OK [0m] Started Login Service. Starting WPA supplicant... Starting Bluetooth service... Starting Set console scheme... [[0;32m OK [0m] Started LSB: Load kernel modules needed to enable cpufreq scaling. [[0;32m OK [0m] Started Set console scheme. [[0;32m OK [0m] Started Bluetooth service. [[0;32m OK [0m] Started WPA supplicant. Starting Hostname Service... Starting LSB: set CPUFreq kernel parameters... [[0;32m OK [0m] Started Hostname Service. [[0;32m OK [0m] Started LSB: set CPUFreq kernel parameters. Stopping LSB: Start busybox udhcpd at boot time... [[0;32m OK [0m] Stopped LSB: Start busybox udhcpd at boot time. [[0;32m OK [0m] Stopped dnsmasq - A lightweight DHCP and caching DNS server. Starting dnsmasq - A lightweight DHCP and caching DNS server... [[0;32m OK [0m] Found device /dev/ttyS0. [[0;32m OK [0m] Started dnsmasq - A lightweight DHCP and caching DNS server. [[0;32m OK [0m] Reached target Host and Network Name Lookups. [[0;32m OK [0m] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch. [[0;32m OK [0m] Started ifup for eth0. [[0;32m OK [0m] Found device /sys/subsystem/net/devices/eth0. [[0;32m OK [0m] Found device /dev/ttyGS0. (1 of 2) A start job is running for...work interfaces (33s / 5min 22s) FAILED[0m] Failed to start Raise network interfaces. See 'systemctl status networking.service' for details. [[0;32m OK [0m] Reached target Network. Starting OpenBSD Secure Shell server... [[0;32m OK [0m] Reached target Network is Online. [[0;32m OK [0m] Started Daily apt download activities. [[0;32m OK [0m] Started Daily apt upgrade and clean activities. [[0;32m OK [0m] Reached target Timers. Starting /etc/rc.local Compatibility... Starting LSB: Advanced IEEE 802.11 management daemon... Starting LSB: Apache2 web server... [[0;32m OK [0m] Started /etc/rc.local Compatibility. [[0;32m OK [0m] Started LSB: Advanced IEEE 802.11 management daemon. [[0;32m OK [0m] Started OpenBSD Secure Shell server. [[0;32m OK [0m] Started Serial Getty on ttyGS0. [[0;32m OK [0m] Started Getty on tty1. [[0;32m OK [0m] Started Serial Getty on ttyS0. [[0;32m OK [0m] Reached target Login Prompts. [[0;32m OK [0m] Started Generic Board Startup. [[0;32m OK [0m] Started LSB: Apache2 web server. [[0;32m OK [0m] Reached target Multi-User System. [[0;32m OK [0m] Reached target Graphical Interface. Starting Update UTMP about System Runlevel Changes... [[0;32m OK [0m] Started Update UTMP about System Runlevel Changes. Ubuntu 16.04.3 LTS arm ttyS0 default username:password is [ubuntu:temppwd] arm login: ubuntu Password: Last login: Tue Aug 14 03:58:34 UTC 2018 on ttyS0 Welcome to Ubuntu 16.04.3 LTS (GNU/Linux 4.14.41-bone14 armv7l) * Documentation: https://help.ubuntu.com * Management: https://landscape.canonical.com * Support: https://ubuntu.com/advantage ubuntu@arm:~$ sudo -s [sudo] password for ubuntu: root@arm:~# mii-tool -v eth0 eth0: negotiated 1000baseT-FD flow-control, link ok product info: vendor 00:07:32, model 17 rev 5 basic mode: autonegotiation enabled basic status: autonegotiation complete, link ok capabilities: 1000baseT-HD 1000baseT-FD 100baseTx-FD 100baseTx-HD 10baseT-FD 10baseT-HD advertising: 1000baseT-FD 100baseTx-FD 100baseTx-HD 10baseT-FD 10baseT-HD link partner: 1000baseT-HD 1000baseT-FD 100baseTx-FD 100baseTx-HD 10baseT-FD 10baseT-HD flow-control root@arm:~# ifconfig eth0 Link encap:Ethernet HWaddr 90:70:65:c4:80:22 inet addr:169.254.143.164 Bcast:169.254.255.255 Mask:255.255.0.0 inet6 addr: fe80::9270:65ff:fec4:8022/64 Scope:Link UP BROADCAST RUNNING MULTICAST DYNAMIC MTU:1500 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:98 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:0 (0.0 B) TX bytes:35108 (35.1 KB) Interrupt:45 lo Link encap:Local Loopback inet addr:127.0.0.1 Mask:255.0.0.0 inet6 addr: ::1/128 Scope:Host UP LOOPBACK RUNNING MTU:65536 Metric:1 RX packets:1928 errors:0 dropped:0 overruns:0 frame:0 TX packets:1928 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:117800 (117.8 KB) TX bytes:117800 (117.8 KB) usb1 Link encap:Ethernet HWaddr 90:70:65:c4:80:27 inet addr:192.168.6.2 Bcast:192.168.6.3 Mask:255.255.255.252 UP BROADCAST MULTICAST MTU:1500 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:0 (0.0 B) TX bytes:0 (0.0 B) root@arm:~# ethtool eth0 Settings for eth0: Supported ports: [ TP MII ] Supported link modes: 10baseT/Half 10baseT/Full 100baseT/Half 100baseT/Full 1000baseT/Half 1000baseT/Full Supported pause frame use: Symmetric Receive-only Supports auto-negotiation: Yes Advertised link modes: 10baseT/Half 10baseT/Full 100baseT/Half 100baseT/Full 1000baseT/Half 1000baseT/Full Advertised pause frame use: No Advertised auto-negotiation: Yes Link partner advertised link modes: 10baseT/Half 10baseT/Full 100baseT/Half 100baseT/Full 1000baseT/Full Link partner advertised pause frame use: Symmetric Link partner advertised auto-negotiation: Yes Speed: 1000Mb/s Duplex: Full Port: MII PHYAD: 1 Transceiver: external Auto-negotiation: on Supports Wake-on: d Wake-on: d Current message level: 0x00000000 (0) Link detected: yes root@arm:~# ethtool -d eth0 Offset Values ------ ------ 0x0000: 00 00 00 00 70 90 00 10 22 80 c4 65 0c 00 00 00 0x0010: ff ff 00 d0 ff ff ff ff 00 00 00 00 00 00 00 20 0x0020: 07 06 07 07 1c 00 00 00 33 33 00 10 01 00 00 00 0x0030: 1c 00 00 00 00 01 00 10 01 00 00 5e 1c 00 00 00 0x0040: 33 33 00 10 22 80 c4 ff 1c 00 00 00 33 33 00 10 0x0050: fb 00 00 00 1c 00 00 00 00 01 00 10 fb 00 00 5e (0x0060~0x2fff):00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 root@arm:/# ping 10.0.0.1 PING 10.0.0.1 (10.0.0.1) 56(84) bytes of data. From 169.254.143.164 icmp_seq=1 Destination Host Unreachable From 169.254.143.164 icmp_seq=2 Destination Host Unreachable From 169.254.143.164 icmp_seq=3 Destination Host Unreachable From 169.254.143.164 icmp_seq=4 Destination Host Unreachable From 169.254.143.164 icmp_seq=5 Destination Host Unreachable From 169.254.143.164 icmp_seq=6 Destination Host Unreachable From 169.254.143.164 icmp_seq=7 Destination Host Unreachable From 169.254.143.164 icmp_seq=8 Destination Host Unreachable From 169.254.143.164 icmp_seq=9 Destination Host Unreachable From 169.254.143.164 icmp_seq=10 Destination Host Unreachable ping: sendmsg: Network is unreachable ping: sendmsg: Network is unreachable ping: sendmsg: Network is unreachable ping: sendmsg: Network is unreachable ping: sendmsg: Network is unreachable ^C --- 10.0.0.1 ping statistics --- 15 packets transmitted, 0 received, +10 errors, 100% packet loss, time 14265ms pipe 4 root@arm:/# root@arm:cd /boot/dtbs root@arm:/boot/dtbs# cd 4.14.41-bone14 root@arm:/boot/dtbs/4.14.41-bone14# ll total 2272 drwxr-xr-x 2 root root 4096 Aug 12 21:26 ./ drwxr-xr-x 3 root root 4096 Aug 11 13:33 ../ -rw-r--r-- 1 root root 60732 Aug 12 06:39 am335x-abbbi.dtb -rw-r--r-- 1 root root 55273 Aug 12 06:39 am335x-baltos-ir2110.dtb -rw-r--r-- 1 root root 55951 Aug 12 06:39 am335x-baltos-ir3220.dtb -rw-r--r-- 1 root root 56154 Aug 12 06:39 am335x-baltos-ir5221.dtb -rw-r--r-- 1 root root 53308 Aug 12 06:39 am335x-base0033.dtb -rw-r--r-- 1 root root 58795 Aug 12 06:39 am335x-boneblack-audio.dtb -rw-r--r-- 1 root root 57675 Aug 12 06:39 am335x-boneblack-bbb-exp-c.dtb -rw-r--r-- 1 root root 57317 Aug 12 06:39 am335x-boneblack-bbb-exp-r.dtb -rw-r--r-- 1 root root 60246 Aug 12 06:39 am335x-boneblack-bbbmini.dtb -rw-r--r-- 1 root root 60811 Aug 14 03:50 am335x-boneblack.dtb -rw-r--r-- 1 root root 60811 Aug 12 06:37 am335x-boneblack-giga.dtb -rw-r--r-- 1 root root 58398 Aug 14 03:51 am335x-boneblack-uboot.dtb -rw-r--r-- 1 root root 58398 Aug 12 06:39 am335x-boneblack-uboot-giga.dtb -rw-r--r-- 1 root root 62547 Aug 12 06:39 am335x-boneblack-wireless.dtb -rw-r--r-- 1 root root 54356 Aug 12 06:39 am335x-boneblack-wl1835mod.dtb -rw-r--r-- 1 root root 54421 Aug 12 06:39 am335x-boneblue.dtb -rw-r--r-- 1 root root 58374 Aug 12 06:39 am335x-bone.dtb -rw-r--r-- 1 root root 58673 Aug 12 06:39 am335x-bonegreen.dtb -rw-r--r-- 1 root root 60529 Aug 12 06:39 am335x-bonegreen-wireless.dtb -rw-r--r-- 1 root root 52115 Aug 12 06:39 am335x-chiliboard.dtb -rw-r--r-- 1 root root 54459 Aug 12 06:39 am335x-cm-t335.dtb -rw-r--r-- 1 root root 60955 Aug 12 06:39 am335x-evm.dtb -rw-r--r-- 1 root root 59043 Aug 12 06:39 am335x-evmsk.dtb -rw-r--r-- 1 root root 55543 Aug 12 06:39 am335x-icev2.dtb -rw-r--r-- 1 root root 52664 Aug 12 06:39 am335x-lxm.dtb -rw-r--r-- 1 root root 54966 Aug 12 06:39 am335x-moxa-uc-8100-me-t.dtb -rw-r--r-- 1 root root 53101 Aug 12 06:39 am335x-nano.dtb -rw-r--r-- 1 root root 55823 Aug 12 06:39 am335x-olimex-som.dtb -rw-r--r-- 1 root root 56318 Aug 12 06:39 am335x-pepper.dtb -rw-r--r-- 1 root root 56880 Aug 12 06:39 am335x-phycore-rdk.dtb -rw-r--r-- 1 root root 129574 Aug 12 06:39 am335x-pocketbeagle.dtb -rw-r--r-- 1 root root 61829 Aug 12 06:39 am335x-sancloud-bbe.dtb -rw-r--r-- 1 root root 56694 Aug 12 06:39 am335x-sbc-t335.dtb -rw-r--r-- 1 root root 54283 Aug 12 06:39 am335x-shc.dtb -rw-r--r-- 1 root root 55455 Aug 12 06:39 am335x-sl50.dtb -rw-r--r-- 1 root root 55647 Aug 12 06:39 am335x-wega-rdk.dtb -rwxr-xr-x 1 root root 60851 Aug 12 21:26 f.dtb* -rwxr-xr-x 1 root root 58438 Aug 12 21:26 f-uboot.dtb* root@arm:/opt# root@ubuntu:/opt# diff bbb.dts f-bbb.dts 879c879 < pinctrl-single,pins = <0x114 0x2 0x118 0x22 0x11c 0x2 0x120 0x2 0x124 0x2 0x128 0x2 0x12c 0x2 0x130 0x22 0x134 0x22 0x138 0x22 0x13c 0x22 0x140 0x22>; --- > pinctrl-single,pins = <0x108 0x28 0x10c 0x28 0x110 0x30 0x114 0x0 0x118 0x30 0x11c 0x0 0x120 0x0 0x124 0x0 0x128 0x0 0x12c 0x30 0x130 0x30 0x134 0x30 0x138 0x30 0x13c 0x30 0x140 0x30>; 885c885 < pinctrl-single,pins = <0x114 0x27 0x118 0x27 0x11c 0x27 0x120 0x27 0x124 0x27 0x128 0x27 0x12c 0x27 0x130 0x27 0x134 0x27 0x138 0x27 0x13c 0x27 0x140 0x27>; --- > pinctrl-single,pins = <0x108 0x27 0x10c 0x27 0x110 0x27 0x114 0x27 0x118 0x27 0x11c 0x27 0x120 0x27 0x124 0x27 0x128 0x27 0x12c 0x27 0x130 0x27 0x134 0x27 0x138 0x27 0x13c 0x27 0x140 0x27>; 2179,2180c2179,2180 < phy_id = <0x48 0x1>; < phy-mode = "rgmii-txid"; --- > phy_id = <0x48 0x0>; > phy-mode = "mii"; root@ubuntu:/opt# diff bbb-uboot.dts f-bbb-uboot.dts 879c879 < pinctrl-single,pins = <0x114 0x2 0x118 0x22 0x11c 0x2 0x120 0x2 0x124 0x2 0x128 0x2 0x12c 0x2 0x130 0x22 0x134 0x22 0x138 0x22 0x13c 0x22 0x140 0x22>; --- > pinctrl-single,pins = <0x108 0x28 0x10c 0x28 0x110 0x30 0x114 0x0 0x118 0x30 0x11c 0x0 0x120 0x0 0x124 0x0 0x128 0x0 0x12c 0x30 0x130 0x30 0x134 0x30 0x138 0x30 0x13c 0x30 0x140 0x30>; 885c885 < pinctrl-single,pins = <0x114 0x27 0x118 0x27 0x11c 0x27 0x120 0x27 0x124 0x27 0x128 0x27 0x12c 0x27 0x130 0x27 0x134 0x27 0x138 0x27 0x13c 0x27 0x140 0x27>; --- > pinctrl-single,pins = <0x108 0x27 0x10c 0x27 0x110 0x27 0x114 0x27 0x118 0x27 0x11c 0x27 0x120 0x27 0x124 0x27 0x128 0x27 0x12c 0x27 0x130 0x27 0x134 0x27 0x138 0x27 0x13c 0x27 0x140 0x27>; 2133,2134c2133,2134 < phy_id = <0x44 0x1>; < phy-mode = "rgmii-txid"; --- > phy_id = <0x44 0x0>; > phy-mode = "mii"; root@ubuntu:/opt#
Steve