This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

ADS7223: CID in full clock mode

Expert 4580 points

Replies: 10

Views: 216

Part Number: ADS7223

Hello Team,

we are using the ADS7223 in full clock mode. Our idea was to read the CID with each conversion for plausibility testing. It seem that in this mode the channel number reported is always "00" when CID = "0" which normally should report the Channel ID as per the description of BIT5 (CID disable) on page 35 of the datasheet. There is a hint above the diagrams on page 27 of the datasheet.

However, is there any way to read the CID when using full clock mode? Or is this feature simply not available in full clock mode?

many thanks

Lutz

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.