Hi all,
Would you mind if we ask TLV320DAC3101?
<Question>
The following is our customer's circuit using TLV320DAC3101.
20150528_TLV320DAC3101.pdf
In this circuit, our customer measured THD+N using attached circuit.
<The result of THD+N>
-400Hz: THD+N 1.4%
-1kHz: THD+N 3.5%
-output power was 50mW
Originally, the higher the frequency increases, the better the value of THD+N will be.
However, it seems that it occurs the opposite phenomenon.
So, if you have some advice, could you let us know it?
Kind regards,
Hirotaka Matsumoto