Hello world, im currently facing a problem that no output sound produced from the DSK6713 board by using speaker.
There is no errors in the codes, but just no output is produce. can i know why? someone help me please.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello world, im currently facing a problem that no output sound produced from the DSK6713 board by using speaker.
There is no errors in the codes, but just no output is produce. can i know why? someone help me please.
Hi,
Thanks for your post.
Are you using TI provided DSK_6713_audio example code or your custom code?
If TI provided, are you using the example code "as-is" or have you modified the code?
If modified, what are the changes have you made to configure the AIC23 codec to output the audio through speakers?
Did you use the example code as the path mentioned below?
~\ti\DSK_c6713_audio\.ccsproject
From my end, the above example seems to work fine, waiting to hear inputs from you.
Thanks & regards,
Sivaraj K
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
--------------------------------------------------------------------------------------------------------
This is my program
i just copy it from online. but it cant work
//Speech Synthesis Using Linear Predictive Coding
#include "DSK6713_AIC23.h"
Uint32 fs= DSK6713_AIC23_FREQ_8KHZ;
#define DSK6713_AIC23_INPUT_MIC 0x0015
#define DSK6713_AIC23_INPUT_LINE 0x0011
Uint16 inputsource=DSK6713_AIC23_INPUT_LINE;
//#include "dsk6713_aic23.h"
//Uint32 fs=DSK6713_AIC23_FREQ_8KHZ;
#include <stdio.h>
#include <math.h>
#include "input.h" /* Holds the input speech samples */
#include "hamming.h" /* Holds the scaled Hamming window coefficients */
#define Def_overlap 40 /* Default overlap length */
#define Def_framelength 80 /* Default frame length */
#define Def_total 7440 /* Total length of the speech samples */
#pragma DATA_SECTION (G_final_output,".output"); /* Store the output in External Memory */
#pragma DATA_SECTION (input,".input"); /* Store the input in External Memory */
int G_index=Def_total+3400; /* Index to the output array */
int G_index2=0;
int *G_final_output=NULL; /* To store the synthesised speech */
int G_out=0;
short dummy=0;
interrupt void c_int11()
{
G_out=G_final_output[G_index];
if (G_index2 % 2 == 0)
{
G_out=0;
G_index++;
}
dummy=input_sample();
output_sample(G_out);
G_index2++;
if (G_index==Def_total*2 )
{
G_index=Def_total+3400;
G_index2=0;
}
}
/**** The display routines can be used to view the contents of various arrays ****/
/**** input: arr:the array to be viewed size: Size of the array ****/
/**** for displaying integer arrays ****/
void display(int* arr,int size)
{
int i;
for( i=0;i<size;i++)
printf("%d\n",*(arr+i));
}
// for displaying float arrays
void dispflt(float* arr,int size)
{
int i;
for( i=0;i<size;i++)
printf("%f\n",*(arr+i));
}
/**** SEGMENTATION FUNCTION ***/
/**** input : start:Index of input array defining the start of the segment *****/
/**** return: segment:pointer to the first element of the segment *****/
/**** This function takes in the starting index and returns a *****/
/**** segment whose length is Def_framelength *****/
int* segmentation(int start)
{
int loop;
int seg_loop=0;
int* segment;
segment=(int *)malloc(sizeof(int)*Def_framelength);
for(loop=start;loop<start+Def_framelength;loop++ )
{
segment[seg_loop]=input[loop];
seg_loop++;
}
return segment;
}
/**** WINDOWING FUNCTION **/
/**** input : sp_input:The array containing the segmented input ****/
/**** return: out:the Hamming windowed segment ****/
/**** The Function takes in the segmented speech samples.The ****/
/**** hamming window coefficients are multipled with the segmented ****/
/**** speech. ****/
int* window(int* sp_input)
{
int loop=0;
int* out;
out=(int *)malloc(sizeof(int)*Def_framelength);
for(loop=0;loop<Def_framelength;loop++)
out[loop]=sp_input[loop]*ham[loop];
return (out);
}
/** AUTOCORRELATION FUNCTION **/
/**** input : sp_input:The array containing the windowed segment ****/
/**** :p : The number of autocorrelation coefficients required ****/
/**** return: corr:Array containing the autocorrelation coefficients ****/
/**** The function takes in the hamming windowed segment and ****/
/**** calculates the autocorrelation coefficients(the number specified***/
/**** by input parameter p)for the segment ****/
int* xcorr(int* sp_input, short p)
{
short i;
int j;
int* corr;
corr=(int*)malloc((sizeof(int)* p));
for(i=0;i<p;i++)
{
corr[i]=0;
// Loop till Def_framelength-i so that index does not spill over
for (j=0;j<Def_framelength-i;j++)
corr[i]=corr[i]+ (sp_input[j]*sp_input[j+i] );
}
return (corr);
}
/**** LPC FUNCTION ****/
/**** input : r:Autocorrelation coefficients *****/
/**** order: The number of LPC coefficients required ****/
/**** return: alpha : LPC coefficients *****/
/**** The function calculates the LPC coefficients of a segment ****/
/**** of speech from the correlation coefficients using Levinson-Durbin Algorithm ****/
float* levinson(int* r, short order)
{
float *e;
float *k;
float *alpha;
float *alpha_prev;
int i=1,j=1 ;
float sum=0.0;
short loop;
e=(float *)malloc((order+1)*sizeof(float));
k=(float *)malloc((order+1)*sizeof(float));
alpha=(float *)malloc((order+1)*sizeof(float));
alpha_prev=(float *)malloc((order+1)*sizeof(float));
// Initialising the Array variables
for (loop=0;loop<order+1;loop++)
{
e[loop]=0;
k[loop]=0;
alpha[loop]=0;
alpha_prev[loop]=0;
}
// End initalising
e[0]=r[0];
// Iterate with i=1 to order as iteration variable
i=1;
for(i=1;i<=order;i++)
{
// start step 1
sum=0;
for (j=1;j<=i-1;j++)
sum+=alpha_prev[j]*r[i-j];
k[i]=(r[i]-sum)/e[i-1];
// End step 1
//start step 2
alpha[i]=k[i];
for(j=1;j<=i-1;j++)
alpha[j]=alpha_prev[j]- ( k[i]*alpha_prev[i-j] ) ;
//end step 2
//start step 3
e[i]=e[i-1]*(1-(k[i]*k[i]));
//end step 3
for( loop=0;loop<order+1;loop++)
{
alpha_prev[loop]=alpha[loop];
}
}// End For levinson
for( loop=0;loop<order+1;loop++)
alpha[loop]=-1*alpha[loop];
alpha[0]=1;
free(alpha_prev);
free(e);
free(k);
return (alpha);
}
/**** RESIDUAL FUNCTION ****/
/**** input : Num_cof: Filter coefficients ****/
/**** Nr_size: Number of filter coefficients ****/
/**** input : speech segment ****/
/**** return: sum_numerator : Output of the filter ****/
/**** The function implements an FIR filter. Output is the residual****/
/**** signal when given the speech segment as the input and the ****/
/**** filter coefficients being the LPC parameters ****/
int* fir_filter(float *Num_cof,short Nr_size,int *fir_input )
{
int loop_var=0;
int i;
int output_loop=0;
int *sum_numerator;
float lpc_copy[18];
for(i=0;i<Nr_size;i++)
lpc_copy[i]=Num_cof[i];
sum_numerator=(int *)malloc((sizeof(int))*Def_framelength);
// numerator
for(output_loop=0;output_loop<Def_framelength;output_loop++)
{
sum_numerator[output_loop]=0;
for(loop_var=0;(loop_var<=output_loop) && (loop_var<Nr_size) ;loop_var++)
{
sum_numerator[output_loop] += lpc_copy[loop_var]*fir_input[output_loop-loop_var];
}
}
return (sum_numerator);
}
/**** SYNTHESIS FUNCTION ****/
/**** input : Den_coff: Filter coefficients ****/
/**** Nr_size: Number of filter coefficients ****/
/**** input : residual speech signal ****/
/**** return: sum_denom : Filter output(synthesised speeech segment ****/
/**** The function implements an IIR filter. Output is the ****/
/**** synthesised speeech segment when given the residual signal ****/
/**** as the input and the filter coefficients being the LPC ****/
/**** parameters ****/
int* iir_filter(float* Den_coff,short Nr_size,int *iir_input)
{
int loop_var=0;
int output_loop=0;
int *sum_denom;
sum_denom=(int *)malloc((sizeof(int))*Def_framelength);
for(output_loop=0;output_loop<Def_framelength;output_loop++)
{
for(loop_var=1;loop_var<output_loop ;loop_var++)
{
sum_denom[output_loop]+= Den_coff[loop_var]*sum_denom[output_loop-loop_var];
}
sum_denom[output_loop]=iir_input[output_loop]-sum_denom[output_loop];
}
return (sum_denom);
}
/***** BUFFERING FUNCTION ****/
/**** input : frame_in: the synthesised speech frame ****/
/**** start : index of starting position ****/
/**** return: void ****/
/**** The function puts all the synthesised speech frames together ****/
/**** to form the final synthesised speech signal ****/
void accumulate(int* frame_in,int start)
{
int loop=0;
int j=0;
for (loop=start;loop<Def_framelength;loop++)
{
G_final_output[loop]=frame_in[j];
G_final_output[loop]=G_final_output[loop]>>15; // Scaling
j++;
}
}
/******************************MAIN FUNCTION********************************/
void main()
{
int loopvar=0;
int *present_seg;
int *corr;
float* lpc;
int *residue;
int *windowed;
int *frame_out;
comm_intr(); // Initializing the DSK and the interrupts
printf("start here");
//Memory Allocation to store Output
G_final_output=(int*)malloc(sizeof(int)*Def_total*2);
// Start of main segmentation
for (loopvar=0;loopvar<=Def_total-Def_framelength;loopvar+=Def_overlap)
{
//Loop iterates for every speech segment.Every speech segment is windowed ***/
//calculate autocorrelation coefficients,LPC parameters,Residual signal from FIR, ***/
//Synthesised frame from passing residual signal->IIR
//frames buffered->G_final_output array
present_seg=segmentation(loopvar);
windowed=window(present_seg); //multiply by contents of hamming
free(present_seg);
corr=xcorr(windowed,10);//calculate autocorrelation
lpc=levinson(corr,9); //calculate LPC coefficients
free(corr);
residue=fir_filter(lpc,10,windowed);//calculate residual signal
free(windowed);
frame_out=iir_filter(lpc,10,residue);//generate synthesized segment
free(residue);
accumulate(frame_out,loopvar); //buffer synthesized segment
free(frame_out);
} // End Of Segmentation loop
printf("\n done \n");
while(1);
}// END OF MAIN PROGRAM
Hi,
You can download BSL and example code from the DSKC6713 support home page as below:
http://c6000.spectrumdigital.com/dsk6713/revc/
For more details on DSK6713 kit includes, please refer below:
http://www.spectrumdigital.com/product_info.php?&products_id=113
Also, please find attached the minimal audio c6713 zip file in which you would be able to extract the c6713 audio example code:
You could also download the CSL for C6713 from the below TI wiki:
http://processors.wiki.ti.com/index.php/C6713DSK_in_CCSv5#Prerequisites
Download CSL @ http://www.ti.com/tool/sprc090
Thanks & regards,
Sivaraj K
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
-------------------------------------------------------------------------------------------------------