Other Parts Discussed in Thread: , LMK04828
Hi,
We are trying to use ADC14X250 to send some data using fiber, SFP+, similar to aronii. I have few questions:
1. If I am trying to test with 1 ADC module with 1 channel and 1 communication link (the conversion protocol is JESD204B, and I have fiber link (SFP+)), I don't need to worry about latency and syncing, hence I don't need the SYSREF input - Am I correct here?
2. ADC14X250 is capable of 250 MSPS, is it possible to operate with lower clock frequency (keeping in mind that it has to be higher than signal freq.)? If yes, how low can I go? User manual recommends signla generator of range 10MHz- 250MHz but does not provide the limitation.
3. The differential output of ADC14X250, SO+ and SO- pins, can they be directly connected to the TX (TD+/-) pins of the SPF+ connector, without any signal conditioning?
I thank you in advance.
Lee