Hi
I have interfaced ADS1293 to EFM32 controller through SPI. Before giving ECG signal I am trying to give input dc voltage to input IN1 after routing it to channel 1. But whatever voltage I give at the input, I get attenuated voltage at the output by calculating the voltage from the formula provided in the datasheet.
For example: If I give 100mv as input I get corresponding output for 45mv. If I give 150mv I get corresponding output for 65mv. Why this is the case? Please assist me..
Note: I tried the test mode provided in the datasheet without giving any input voltage. In that case the output is coming perfectly fine for all the channels of 0.2V.
Thanks
Arnab Chakraborty