Could you please check out this schematic that I edited based off of the schematic from Evaluation board and Datasheet together I will supply +-15V externally.
Let me give you some information related the product: We are going to control Hydraulic actuators that works with +-10V & 0-20mA & 4-20mA & 0-24mA control signals , We will use more than one DAC8760 together on Daisy Chain mode (SPI) and also we are planning to add 24 bit ADC later to our system for feedback purpose. We appreciate any consultation.
Since we are planning to control Hydraulic actuators we don't want to come across with any oscillation problem, I cancel the boost configuration, and decide to remove it from schematic.
We decide to use DAC8760 on dual out mode, After some warning related with Vsense+ I have used OPA188ADBVT for protection reverse current from IOUT, I believe this way it is more protected from reverse current. I got the information from datasheet of DAC8760 related with VSENSE+ and DualOut case.
I appreciate any advice or consultation about the appropriate design especially related with IEC61000-4 , ESD, EFT tests.
We will expose the design to industrial transients such as the IEC61000-4 suite
Certification life cycle really needs to start early in the life cycle of a device so any consultation is appreciated from the beginning of this process. After controller attached to the system together on the same board we need to get IEC61000-4 , and also pass ESD and EFT tests.
With your comments and improvements I will change the schematic. and then begin careful layout for EMC I basically capture EVB board and connect the jumpers to proper pins and remove them out from the schematic, such as CLR-SEL -DVDD - REFIN / REFOUT and +Vsense I have some more questions as well regarding the Hart Communication pin etc.
i -) Do i need to connect Hart pin to 0.0022u capacitor? It is hard to layout the +Vsense pin on the pcb close enough when I add a capacitor to Hart pin, if it doesn't make any oscillation when hart is off mode, I would like to live Hart pin float, or connect directly to ground if it is possible.
ii -) From Respect to "tidu392.pdf referance desing" : Do i need any pull ups or direct Resistors (like R4 on my schematic) on the SPI lines? Could you help me understand the reason we use 10ohm resistor serial to the SDO pin. on my previous designs I basically connect them together without any resistor serial on the SDO (like R4).
Thank you for your answers and recommendations.
Best Regards.