Hi,
I am new to the design of DAC8760 while designing there i a short between AVSS, Thermal Pad and analog ground. Due to this error can't use bipolar. And need to know when the Iout Loading or Compliance voltage violation bit is set, how can the issue be solved. I have checked in Avdd that I'm providing 12V and Avss to Ground (due to the above reason we have done connection like that). Moreover I am using multi-meter to measure the curremt so my load will be 250 ohms. Will the current be driven for that load normally or I have to add more resistance like 1kohm to it? Because the ALARM pin is Set Low and while reading the Status bit getting the data as 4 which means "Iout loading or Compliance voltage Violation bit is set".
Please can anyone tell me the solution to identify the erros
Thanks,
Gokul.