Other Parts Discussed in Thread: MSP430F5438, , MSP-EXP430F5529LP
Tool/software: Code Composer Studio
Hello,
I'm using ADS1247 with a msp430f5438 microcontroller, and i'm having issues with the spi communication. I've connected START and RESET pins to gpio and I put them at high level at the beginning of my code, while CS pin is tied low.
Then I try to read/write registers of the ADS1247 and i'm not having any answer from the MISO. The device is correctly powered, I can see DDRY pin going high at the default rate of 5 sps. But even if I try to change the data rate in SYS0 register, the data rate keeps at 5 sps.
Am i doing something wrong ? Why can't i have an answer on SPI communication ?
Here are shots of the logical analyser where we can see the DRDY pulses and then a shot where i'm trying to change the data rate and nothing changes.