I try to use TVP5158 connect with FPGA and the Camera operate in PAL mode (Check by connect with TV). And I have many problem so please suggest me.
1. After power on, default mode of TVP5158 operate in CVBS Autoswitch mode and when check in regsiter 0x0C, it return 0x01 that means NTSC mode. And the register 0x00 = 0x10 which is not lock Vsync and HSync. Why it can't detect PAL mode? Does it has some mistake? (I already set regster 0xb2 = 0x25)
2. when I try to set register 0x0d = 0x02 to force operate in PAL mode, I still get register 0x00 = 0x70, why it is not lock VSync and HSync?. Do I set some register mistake to operate in PAL mode, please suggest me?