This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, all
There are two problems in TPS61194's circuit:
1. When LED_BL don't connect with any LEDs, the voltage of LED_BL change to 13V from 27.6V, but, the EVM's circuit is aways 30V. Why?
2.When LED_BL connect with LEDs,OUT1/2/3 is 80mA, but the SW pin's wave of TPS61194 is abnormal,like the picture.Is not continuous wave?