This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All,
In DM385 IPNC RDK V3.5.0 make file, 256MB and 512MB compilation option is available.In DM385IPNC 2 x16 ddr3 connected to EMIF0 and default ddr3 frequency is 533Mhz. I have changed ddr3 frequency to 266Mhz. and I have compiled RDK using 256MB option. With this change IPNC RDK (all application) working fine. I have disabled x16 256MB ddr3 @ D15-D31 using (#define DDR3_EMIF_SDRAM_CONFIG 0x61C15A32) in u-boot. But after disabling ddr3 @ D15-D31 we are getting below error from m3vpss.
Why m3vpss is giving this error? How to interface DDR3 to EMIF for 256MB DDR(@266Mhz)?
Case 1: x16 256MB --> EMIF0 D0-D15
Case 2: x16 128MB --> EMIF0 D0-D15 & x16 128MB --> EMIF0 D16-D31
Case 3. x32 256MB --> EMIF0 D0-D31
Which case we can use for 256MB interface?
Error:
[m3vpss ] ##################### REISZER OVERFLOW OCCURED: RESTARTING...############################
[m3vpss ] ##################### REISZER OVERFLOW OCCURED: RESTARTING...############################
[m3vpss ] 7124: CAMERA: Overflow detected on VP0, Total Resets = 6
[m3vpss ] 7125: CAMERA: Overflow detected on VP1, Total Resets = 6
mkdosfs 3.0.12 (29 Oct 2011)
unable to get drive geometry, using default 255/63
/dev/sbulla has 255 heads and 63 sectors per track,
logical sector size is 512,
using 0xf8 media descriptor, with 1024 sectors;
file system has 2 12-bit FATs and 4 sectors per cluster.
FAT size is 1 sector, and provides 247 clusters.
There is 1 reserved sector.
Root directory contains 512 slots and uses 32 sectors.
Volume ID is dea59f6c, no volume label.
[m3vpss ] ##################### REISZER OVERFLOW OCCURED: RESTARTING...############################
[m3vpss ] ##################### REISZER OVERFLOW OCCURED: RESTARTING...############################
[m3vpss ] ##################### REISZER OVERFLOW OCCURED: RESTARTING...############################
[m3vpss ] 7456: CAMERA: Overflow detected on VP0, Total Resets = 7
[m3vpss ] 7457: CAMERA: Overflow detected on VP1, Total Resets = 7
Regards,
Tejash Patel
Tejash,
This means that the FIFO (RSZ) is going into overflow condition often, this will happen if there is not enough bandwidth available to run your use-case.
In this case either increase DDR clock/width or reduce the processing requirements.
Regards
Rajat