I'm using old version CCS3.2.
To speed up the ethernet, I created a larger heap in DDR, and used
bios.MEM.MALLOGSEG = prog.get("DDR");
bios.MEM.BIOSOBJSEG = prog.get("DDR");
to make NDK use the buffer in DDR heap.
However, I found the local variables within each function are also assigned to DDR which is not my desire.
Is there any way to relocate the NDK buffer to DDR, and keep the local variables still in IRAM?
I tried
bios.MEM.STACKSEG = prog.get("IRAM");
bios.TSK.STACKSEG = prog.get("IRAM");
Doesn't work.
Thanks