Today when I launched CCS6.1, it offered an update of MSP430 related stuff (I don't recall exactly how it was phrased.). Now there aren't any "Example Projects" for my part (MSPi2xxx) in the TI Resource Explorer. I know there used to be some, because I've run one -- testblink (I don't know if that was the original name or not) which is still in my workspace.
When I ran the update today, it said I needed to re-launch CCS for the changes to take effect. I did that, and when CCS started up again I was asked for an administrator ID and password, which I gave. It chugged away for a minute or two, but then it bombed because I didn't have proper permissions or something along those lines.
I logged out of my user account and into the administrator account to run the update there, but I couldn't find the EXE file anywhere on the disk (including my user account directories). So I launched CCS from the administrator account, but there was no pop-up about the update. I clicked "Help:Check for Updates" and it said the installation was up to date.
FYI, I'm using:
- Windows 7 Ultimate SP1
- CSS version 6.1.0.00104
Below are some screen caps from TI Resource Explorer.
Thanks.