Hello,
I have configured CCS v6.1 to use spaces instead of tabs, which is under General -> Editors -> Text Editors -> Insert spaces for tabs (element checked). The problem I am now facing is the autocomplete (e.g., when I type "if ()" with a return, press "{" then press enter once more which aligns the "{" under the "if" and places the ending "}" two lines below. these all use tabs instead of space.) it uses tabs and not spaces. How do I configured CCS autocomplete to use spaces and not tabs in these cases.
Regards,
Mark