I have a design simulation based on the LM3671 and a pole is to be created at 45kHz using equation 9 in the datasheet. When I calculate for the capacitor I get 6.8pF but when you input the following parameters for the design
Vin: 3.7-4.2V
Vout: 3.1V
Iout: 0.1A
It calculates C1 at 10pF. Is this a mistake in Webench or am I missing something?
Thanks,
George